Issues After Updating MCUXpresso IDE v11.7.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues After Updating MCUXpresso IDE v11.7.0

710件の閲覧回数
judywatson
Contributor I

Hello everyone,

I recently updated MCUXpresso IDE v11.7.0 on my new AI computer and have been running into several issues since then. The previous version was working fine, but after updating, I’ve encountered the following problems:

  1. Installation Errors: During the update to MCUXpresso IDE v11.7.0, I encountered a few error messages, and it seems like the installation didn’t fully complete as expected. Has anyone else had trouble installing this version on newer systems?

  2. Performance Issues: After updating, the IDE is much slower, particularly when compiling or running large projects. My system should be more than capable of handling this workload, so I’m unsure why it's happening.

  3. Debugging Freezes: When debugging, the IDE often freezes or crashes, especially when using peripheral tools. This wasn’t an issue before the update, so I’m wondering if there’s something specific to v11.7.0 causing this.

I’ve tried reinstalling MCUXpresso and updating my system drivers, but the issues remain. Has anyone else faced similar problems with MCUXpresso IDE v11.7.0, particularly on AI-powered PCs? Any help with troubleshooting would be appreciated!

Thanks in advance!

0 件の賞賛
返信
2 返答(返信)

590件の閲覧回数
SangwooJi
Contributor I

 Thank you for the good information. Cristian. 

0 件の賞賛
返信

698件の閲覧回数
cristiantepus
NXP Employee
NXP Employee

Hi,

IDE 11.7.0 is quite old. Can you try updating to a newer version? The latest is 24.9.

Regards,

Cristian