Issues After Updating MCUXpresso IDE v11.7.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues After Updating MCUXpresso IDE v11.7.0

643 Views
judywatson
Contributor I

Hello everyone,

I recently updated MCUXpresso IDE v11.7.0 on my new AI computer and have been running into several issues since then. The previous version was working fine, but after updating, I’ve encountered the following problems:

  1. Installation Errors: During the update to MCUXpresso IDE v11.7.0, I encountered a few error messages, and it seems like the installation didn’t fully complete as expected. Has anyone else had trouble installing this version on newer systems?

  2. Performance Issues: After updating, the IDE is much slower, particularly when compiling or running large projects. My system should be more than capable of handling this workload, so I’m unsure why it's happening.

  3. Debugging Freezes: When debugging, the IDE often freezes or crashes, especially when using peripheral tools. This wasn’t an issue before the update, so I’m wondering if there’s something specific to v11.7.0 causing this.

I’ve tried reinstalling MCUXpresso and updating my system drivers, but the issues remain. Has anyone else faced similar problems with MCUXpresso IDE v11.7.0, particularly on AI-powered PCs? Any help with troubleshooting would be appreciated!

Thanks in advance!

0 Kudos
Reply
2 Replies

523 Views
SangwooJi
Contributor I

 Thank you for the good information. Cristian. 

0 Kudos
Reply

631 Views
cristiantepus
NXP Employee
NXP Employee

Hi,

IDE 11.7.0 is quite old. Can you try updating to a newer version? The latest is 24.9.

Regards,

Cristian