Hi All,,, I'm hopping someone will give me some insite.. I am needing to use the MCUXpresso IDE v11.1.0_3209 to build / analyze a project.. I have added the SDK for a NXP FRDM-KL46Z Development Board, This worked... Now I have a device (Broadcom AFBR-S50MV85G) that also has an SDK for the development board mentioned above.. How can I tell
MCUXpresso to use the SDK Development Board and the SDK for the BroadCom device... Or how would I handle such a situation... The goal here is to get the broadcom examples working, analyze the demo, the .srec the oscilloscope traces etc, I need to use MCUXpresso to examen the examples, and see what pins are being accessed on the Development board... Any insite would be deeply appreciated.. Thanks...