Import LPCopen project to GNU Eclipse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Import LPCopen project to GNU Eclipse

1,608 Views
ramazan_kurban3
Contributor III

I use LPC1769 on GNU Eclipse. There are many examples for LPCExpresso. How can I import project in LPCopen to Eclipse ? 

3 Replies

1,274 Views
ramazan_kurban3
Contributor III

Is there any limitation ? Is it free complately ? Do I need purchase any license ?

0 Kudos
Reply

1,274 Views
soledad
NXP Employee
NXP Employee

Hi, 

MCUxpreeso is free and it has no code size limit restriction for debugging.

LPCOpen packages that are already available continue to be maintained, and can be used with MCUXpresso IDE. 

You can download MCUXpresso from the following link: 

MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE) | NXP 

I hope this helps, 

Have a nice day!

Regards

Soledad

1,274 Views
BlackNight
NXP Employee
NXP Employee

I suggest that you use the MCUXpresso IDE which has replaced the legacy LPCXpresso IDE.

Erich