I can't get the Project Explore Window up .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can't get the Project Explore Window up .

Jump to solution
1,231 Views
jmanning
Contributor I

I can't get the Project Explore Window up .... When I go Window | Show View | there is not option for Project Explorer, not even under the option Other.

 

0 Kudos
1 Solution
1,209 Views
jmanning
Contributor I

Opening a new workspace brought back the option for Window | Show View |  Project Explore

Thank you !!!!!!!!!!!!!!!!

 

P.S. the reset perspective did not work

View solution in original post

0 Kudos
3 Replies
1,221 Views
ErichStyger
Senior Contributor V

Could you provide more details, please?

For example: which IDE version are you using?

Screenshots of what you see?

ErichStyger_0-1656566500479.png

 

And did you install any special plugins, or is this just a fresh install?

 

1,210 Views
jmanning
Contributor I

Opening a new workspace brought back the option for Window | Show View |  Project Explore

Thank you !!!!!!!!!!!!!!!!

 

P.S. the reset perspective did not work

0 Kudos
1,227 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

How about Reset Perspective: 

 

Alice_Yang_0-1656559120326.png

If still can't work, close the IDE, open it with new workspace.

 

 BR

Alice

 

0 Kudos