I installed MCUXpressoIDE and the proper SDK's, I am using an old version FDRM KL25Z board, I connected it to my laptop with Windows 7 and it is recognized and seems like it has a precharged project with accelerometer because the color led changes according to positions, the green led is also blinking. My computer recognized the board as a device but in the device manager I have this...
Device manager
The problem is that I can't debug any project, the error message is the following:
Error message at debuging
I have already updated the openSDA firmware with 118 version so now it is named BOOTLOADER but I can't debug yet.