How to write to SDRAM on K65 using MCUXpresso IDE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to write to SDRAM on K65 using MCUXpresso IDE?

ソリューションへジャンプ
1,386件の閲覧回数
joseph_jean-jac
Contributor III

Hello Everyone,

I am trying to find out how to write to the 64 Mb SDRAM on the K65 using MCUXpresso IDE? I been using the 256 kb SRAM and I believe that is why I am running into the following issue: "FreeRTOS does not have enough memory in the heap to start the kernel".

As usual, any help is greatly appreciated!

Thanks!

0 件の賞賛
返信
1 解決策
1,251件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Joseph,

K65 hasn't internal SDRAM. But it has a SDRAM controller. To get SDRAMC demo, please download K65 SDK from Welcome | MCUXpresso SDK Builder .

The demo is in SDK_2.2_TWR-K65F180M\boards\twrk65f180m\driver_examples\sdramc

Regards,

Jing

元の投稿で解決策を見る

2 返答(返信)
1,252件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Joseph,

K65 hasn't internal SDRAM. But it has a SDRAM controller. To get SDRAMC demo, please download K65 SDK from Welcome | MCUXpresso SDK Builder .

The demo is in SDK_2.2_TWR-K65F180M\boards\twrk65f180m\driver_examples\sdramc

Regards,

Jing

1,251件の閲覧回数
joseph_jean-jac
Contributor III

I should have mentioned I have to the twr-k65 which does has internal SDRAM, specifically 64 Mb. 

Thank you for pointing out the SDK demo that has code already written to configure the SDRAM for reading and writing. 

0 件の賞賛
返信