Inside MCUXpresso-IDE:
* when we click "Import SDK examples", we see many examples but not DSP examples!
* I check folder: ........\SDK_2.2_TWR-K60D100M\CMSIS\DSP_Lib\Examples
--- I saw *.uvoptx/.uvprojx files
So, can we import DSP examples in MCUXpresso-IDE? or we need to use Keil uVision?
Thanks!
Jerry
已解决! 转到解答。
Hello Jerry,
You can install Keil to run the DSP examples,
or if you want use MCUXpresso IDE, please refer to the below DOC to use CMSIS-DSP,
it introduce the steps on kds, while it is the same with MCUXpresso IDE.
Adding CMSIS-DSP Library to a KSDK 2.x project in Kinetis Design Studio
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Jerry,
You can install Keil to run the DSP examples,
or if you want use MCUXpresso IDE, please refer to the below DOC to use CMSIS-DSP,
it introduce the steps on kds, while it is the same with MCUXpresso IDE.
Adding CMSIS-DSP Library to a KSDK 2.x project in Kinetis Design Studio
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------