How does debugger's Heap Usage (FreeRTOS) tab work?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How does debugger's Heap Usage (FreeRTOS) tab work?

跳至解决方案
4,029 次查看
kackle123
Contributor IV

Looking at the MCUXpresso screen shot, I have a 125 kB FreeRTOS heap.  The tab's graphic says it's fine, but the tab's list seems to show that it's all used up if I add up the numbers.  Am I reading it incorrectly? 

Also, what does "Allocated" mean when that particular memory block is NOT designated to  FreeRTOS task like the others?

0 项奖励
回复
1 解答
3,100 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @kackle123,

1. It can't, this is why I mention that it is probably a bug. Please try updating to the latest IDE version and try again.

2. FreeRTOS also requires heap resources besides the ones reserved for each task, this is why there are some sections that are marked as "Allocated".

BR,
Edwin.

在原帖中查看解决方案

0 项奖励
回复
7 回复数
3,450 次查看
kackle123
Contributor IV

Hi Edwin,

It is a Kinetis K64 MCU (MK64FN1M0VLQ12).  The MCUXpresso is version 11.6.  The SDK, v2.11.0 and manifest v3.9.0.

0 项奖励
回复
3,384 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @kackle123,

Thanks for the clarification. You are reading the tab's list correctly; I believe there might be a bug or error with the graphic instead. That said, the IDE version that you are using is about two years old by now, and many improvements have been made to the FreeRTOS related windows. Please update to the latest MCUXpresso IDE (Currently v24.9) and try again.

BR,
Edwin.

0 项奖励
回复
3,380 次查看
kackle123
Contributor IV

How can the FreeRTOS dynamic memory allocator give out more than 135 kB if the heap was only configured for 125 kB (configTOTAL_HEAP_SIZE)?

Repeating my second question: What does "Allocated" mean when that particular memory block is NOT designated to FreeRTOS task like the others?

 

 

0 项奖励
回复
3,101 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @kackle123,

1. It can't, this is why I mention that it is probably a bug. Please try updating to the latest IDE version and try again.

2. FreeRTOS also requires heap resources besides the ones reserved for each task, this is why there are some sections that are marked as "Allocated".

BR,
Edwin.

0 项奖励
回复
3,097 次查看
kackle123
Contributor IV

As far as updating the IDE, I may not be able to do that until the project is complete (very soon).

The declared allocations explanations make sense.  Thank you for your replies.

 

0 项奖励
回复
3,993 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @kackle123,

Could you share what MCU are you using? Also, the IDE and SDK versions that you are currently working with.

BR,
Edwin. 

0 项奖励
回复
3,434 次查看
kackle123
Contributor IV

(Sorry, I replied in the wrong place.)

Hi Edwin,

It is a Kinetis K64 MCU (MK64FN1M0VLQ12).  The MCUXpresso is version 11.6.  The SDK, v2.11.0 and manifest v3.9.0.

 

0 项奖励
回复