Hi,
I want to use MCUXpresso to develop my Hexiwear.
What I want to do is creating new app on Hexiwear.
So, I need entire source codes for that and I got them from Github.
But as you know, those source codes are based on KDS(Kinetis Design Studio) so that it does not work on MCUXpresso.
MCUXpresso provides basic demo source codes for Hexiwear but that is not what I need.
What shoud I do? And where can I get Hexiwear program source codes for MCUXpresso.
Hi,
There is no straight-forward way for this, basically you have two options:
- create a new project with the IDE and then add the source files
- or use the approach described in MCUXpresso IDE: Importing Kinetis Design Studio Projects | MCU on Eclipse
I hope this helps,
Erich
Erich Thanks for giving me those options!
I want to ask something about first option. Could you let me know what sources are exactly I should add on new project to work factory setup?
If you create a new 'empty' project for the Hexiwear using the IDE and the SDK, basically you get the main with the startup code. Keep the startup code with the main and add the your other project sources.
I hope this helps,
Erich
And What Should I do for thoes error?
Even if head files are in source folder they do not find it if they are not exact same directory.
Thanks
It seems to me that you have not configured correctly the settings for the include path (-I option) in the project settings.
Make sure that the folder with that header file is present in the list.
I hope this helps,
Erich
Hi Erich,
I think I set that path.
But those errors still have come up.
When I try to move each header file that is in inc to src that parts passed. But I have so many header files that is not existed exactly same folder with .c file. So it is not possible to move each ones.
Do you think I make a mistake to set the path?? What is wrong with this?
Thanks Erick.
But I got the error
_cr__main.c:(.text.__main+0xa): undefined reference to `main'
like this.
What can I do for this?