Flash driver file not found error on FRDM-KW36 SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash driver file not found error on FRDM-KW36 SDK

Jump to solution
4,207 Views
ConstYu
NXP Employee
NXP Employee

I am debug FRDM-KW36 board with MCUXpresso IDE v10.2.1 [Build 795] [2018-07-25], but it shows Flash driver file not found error when download the app with on-board cmsis-dap, the error information is as below, any advice?thanks.

Capture.PNG

Labels (1)
0 Kudos
Reply
1 Solution
3,957 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Const, I hope you're doing well,

 

Could you please try downloading the MCUXpresso installer directly from the download page? Some important bugs were fixed in the 10.3.1 version.

 

Best regards,

Sebastian

View solution in original post

6 Replies
3,957 Views
ConstYu
NXP Employee
NXP Employee

The problem is solved after un-install the old version and then re-install the V10.3 version

0 Kudos
Reply
3,957 Views
guilherme_pastr
Contributor I

Hello!

I have the same problem in 10.3.1 version.

0 Kudos
Reply
3,957 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Could you please help us with more details on your problem ? 

Regards, 

Estephania 

0 Kudos
Reply
3,957 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Const, I hope you're doing well,

 

Could you please update to the latest version of MCUXpresso (v10.3.1) and check to see if you're still getting the same error?

 

Best regards,

Sebastian

0 Kudos
Reply
3,957 Views
ConstYu
NXP Employee
NXP Employee

Hi Sebastian,

Thanks for your advice, i tried to update the version by click help->check for update, but it show no any update.

does it mean i must uninstall the version V10.2, then install V10.3? 

Capture.PNG

from the previous error information, looks there is no flashloader support. not sure whether they are related.

Capture1.PNG

0 Kudos
Reply
3,958 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Const, I hope you're doing well,

 

Could you please try downloading the MCUXpresso installer directly from the download page? Some important bugs were fixed in the 10.3.1 version.

 

Best regards,

Sebastian