Flash driver file not found error on FRDM-KW36 SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash driver file not found error on FRDM-KW36 SDK

ソリューションへジャンプ
4,242件の閲覧回数
ConstYu
NXP Employee
NXP Employee

I am debug FRDM-KW36 board with MCUXpresso IDE v10.2.1 [Build 795] [2018-07-25], but it shows Flash driver file not found error when download the app with on-board cmsis-dap, the error information is as below, any advice?thanks.

Capture.PNG

ラベル(1)
0 件の賞賛
返信
1 解決策
3,992件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Const, I hope you're doing well,

 

Could you please try downloading the MCUXpresso installer directly from the download page? Some important bugs were fixed in the 10.3.1 version.

 

Best regards,

Sebastian

元の投稿で解決策を見る

6 返答(返信)
3,992件の閲覧回数
ConstYu
NXP Employee
NXP Employee

The problem is solved after un-install the old version and then re-install the V10.3 version

0 件の賞賛
返信
3,992件の閲覧回数
guilherme_pastr
Contributor I

Hello!

I have the same problem in 10.3.1 version.

0 件の賞賛
返信
3,992件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Could you please help us with more details on your problem ? 

Regards, 

Estephania 

0 件の賞賛
返信
3,992件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Const, I hope you're doing well,

 

Could you please update to the latest version of MCUXpresso (v10.3.1) and check to see if you're still getting the same error?

 

Best regards,

Sebastian

0 件の賞賛
返信
3,992件の閲覧回数
ConstYu
NXP Employee
NXP Employee

Hi Sebastian,

Thanks for your advice, i tried to update the version by click help->check for update, but it show no any update.

does it mean i must uninstall the version V10.2, then install V10.3? 

Capture.PNG

from the previous error information, looks there is no flashloader support. not sure whether they are related.

Capture1.PNG

0 件の賞賛
返信
3,993件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Const, I hope you're doing well,

 

Could you please try downloading the MCUXpresso installer directly from the download page? Some important bugs were fixed in the 10.3.1 version.

 

Best regards,

Sebastian