FRDM KW41Z DATA TRANSFER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM KW41Z DATA TRANSFER

717 Views
jalalbeladel
Contributor II

Hello,

I have coupled the two Transceivers FRDM KW41Z like the example on the nxp page ! I have a communication and if i press the Switch 4 or 3 of the one Transceiver lights up the LED of the other one Transceiver ( This is very good until now). Now when i ímport the LED example and debug it, lights up the LED only on one Transceiver and both Transceiver disconnected from the Ntetwork? i want only to run an application on one Transceiver an see it bei the other one! what can i do?

Thanks.

Tags (1)
0 Kudos
Reply
1 Reply

621 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Which specific LED example are you using?  If you are using a example that it’s on the driver or demo application you won’t be able to keep the connection as those do not have the wireless support nor for BLE or Thread.

If you are using a wireless demo, do you have a sniffer to verify if the packet has been sent?

Best Regards,

Estephania

0 Kudos
Reply