Error when import SDK zip into MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error when import SDK zip into MCUXpresso IDE

1,045 Views
Fan_xy
Contributor III

Hello,

 

CUXpresso IDE v10.1.0 [Build 589] [2017-11-14]

and also

MCUXpressoIDE_10.1.1_606.exe

FRDM-K64-AGM04 SDKv2.3

my system is win10 pro.

 

When import the SDK zip package into MCUXpresso IDE, it shows erro :

pastedImage_1.png

 

What am I missing ?

 

(I have submit the same question on this thread https://community.nxp.com/thread/466986 )

Thank you very much!

Fan

0 Kudos
Reply
1 Reply

916 Views
lpcxpresso_supp
NXP Employee
NXP Employee

What is your exact username on your PC? The username is used by the IDE to provide the location used to install part support information extracted from the SDK. From the errors you are seeing we suspect your issues is related to "an unusual character", maybe an "&", in your username. 

In which case, the only workaround we can think of for the moment is to use the IDE under an alternative username.

 

I apologise for the inconvenience and we will look into solving this issue in a future release.

Regards,

MCUXpresso IDE Support

0 Kudos
Reply