Hello Experts,
I want to download the demo of "evkmimxrt1050_demo_apps_hello_world_xip" into Hyperflash ,
use DAPlink CMSIS-DAP on board, while it failed. I attached the error.
I also refer to the DOC https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide/blog/2017/12/07/overview-of-using-the-... create a new project , while when download , it also failed.
The SW7 on my board has configured to 0110 .
My board is IMXRT1050-EVKB board.
Any help will be appreciate.
Thanks!
Solved! Go to Solution.
Make sure that you have downloaded the SDK for the EVKB board, not the EVK, from mcuxpresso.nxp.com.
As well as various changes between the boards and the silicon revisions which the updated SDK has to allow for, your debug log shows that you are using the flash driver from the original EVK SDK - which is not compatible with the EVKB board.
Regards,
MCUXpresso IDE Support
Make sure that you have downloaded the SDK for the EVKB board, not the EVK, from mcuxpresso.nxp.com.
As well as various changes between the boards and the silicon revisions which the updated SDK has to allow for, your debug log shows that you are using the flash driver from the original EVK SDK - which is not compatible with the EVKB board.
Regards,
MCUXpresso IDE Support
Hello MCUXpresso IDE Support,
Thanks a lot !
It worked now .