Does MCUXpresso IDE v11.8.0 [Build 1165] support for Windows 11(64b) ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MCUXpresso IDE v11.8.0 [Build 1165] support for Windows 11(64b) ?

1,786 Views
Fukui_wb
Contributor I

Does the downloaded module have the new linkServer device driver ?

I also see the https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso55S69-debugger-not-open-in-Windows11-MCUXpress... page.

I have experience almost the same error dialog.

I want to debug, but it seems like the driver doesn't work properly and crashes.

0 Kudos
Reply
4 Replies

1,268 Views
kar1
Contributor I

Hello,

I have same issue on Windows 11, I use v11.9.0 Mcuxpresso, no terminal function

Re: nothing in terminal view for debugging. - NXP Community

Does anybody have ideas?

Waste 4 days to try to solve this issure...

Regards,

 

0 Kudos
Reply

1,740 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Fukui_wb 

MCUXpresso IDE v11.8.0 supports Windows 1164b).

Alice_Yang_0-1693985415621.png

 

Which chip do you use? What about your detail steps and issue? You can take screenshots to show.

 

BR

Alice

0 Kudos
Reply

1,680 Views
Fukui_wb
Contributor I

I'm using NXP LPC54005.

BR

0 Kudos
Reply

1,666 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Fukui_wb 

MCUXpresso IDE 11.8 supports this part.

You can try to change to a new workspace, and create a simple new project to test.

If still has issue, please take screenshots to show your detail steps.

 

 

BR

Alice

0 Kudos
Reply