Disable creation of TAD folders (e.g. "FreeRTOS_TAD_log") if no operating system is used

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable creation of TAD folders (e.g. "FreeRTOS_TAD_log") if no operating system is used

3,959 Views
SynBilly
Contributor III

I'm using MCUXpresso for LPC55xx ("baremetal" application)

MCUXpresso creates the following folders on my hard disk even though I am not using an operating system:

- ZephyrRTOS_TAD_logs

- FreeRTOS_TAD_logs

- AzureRTOS_TAD_logs

How can I disable the "auto creation" of these folders/files?

0 Kudos
Reply
10 Replies

3,943 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

Could you tell me the full number of your MCU?
Could you share an image of the route of these files? I will try if it is possible to lock the creation.

Best regards,
Pavel

0 Kudos
Reply

3,928 Views
SynBilly
Contributor III

Hi,

my MCU-version:   MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13]

The folders are as @ErichStyger stated (located in the workspace folder):

Folders.png

Best regards, Andreas

0 Kudos
Reply

3,898 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Currently there is no switch exposed in the UI for controlling this. Logs associated with active debug session are saved in the folders you noticed, once the debug session is ended. Note that only the most recent 4 logs (if I remember correctly) are kept.

Are those folders interfering in any way with your work/projects? Maybe we can plan adding a preference that controls the logging mechanism for each RTOS plugin.

Regards,
MCUXpresso IDE Support 

0 Kudos
Reply

3,799 Views
SynBilly
Contributor III

Dear NXP,

no, those folders do not interfer the function of our project in any way - it's just a "cosmetic issue".
But it would still be nice if the user could turn off the generation of these folders when they are not needed.

You wrote "there is no switch in the UI...".
-> Is there a switch in the ".metadata" folder or somewhere else?

Best regards, Andreas

0 Kudos
Reply

3,783 Views
lpcxpresso_supp
NXP Employee
NXP Employee

I'm sorry but there's no way to avoid those files/folders. I logged an internal ticket to track your request. Hopefully, it'll be addressed in the next release.

Regards,

MCUXpresso IDE Support

3,217 Views
robertmorrison
Contributor II

I would also like to make these TAD logs optional. It is a waste of SSD write endurance in my case.

0 Kudos
Reply

3,078 Views
ErichStyger
Specialist I

Hi @robertmorrison ,

I wrote in https://mcuoneclipse.com/2023/01/25/nxp-mcuxpresso-ide-11-7-0/ about how you can make the TAD logs optional or disabled.

I hope this helps,

Erich

3,052 Views
robertmorrison
Contributor II

Hi Erich,

   Excellent! I tried this and it works--and in 11.8 they have added a general option to turn off creation of the logging console as well as the logging messages. Now the build console is at the top of the list, the one I most often need to see. This post also has a whole lot of other stuff I found very useful.

  I'm delighted that NXP seems to really work to make mcuxpresso work well and to constantly improve it--I've been with it since the lpcxpresso days and the reliability and usability has seen massive improvement.

Robert

3,044 Views
ErichStyger
Specialist I

Hi Robert,

yes, I noticed that option now too and disabled the console(s) on my side.

Erich

0 Kudos
Reply

3,936 Views
ErichStyger
Specialist I

Hi @Pavel_Hernandez ,

the MCU used does not matter at all: these files are created by the IDE for every device, in the workspace folder:

ErichStyger_0-1664423218285.png

 

 

Erich

0 Kudos
Reply