Creation of MCUxpresso project to boot the code from SDRAM of imxrt1170 evk board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Creation of MCUxpresso project to boot the code from SDRAM of imxrt1170 evk board

3,699 次查看
Jeevan
Contributor IV

Hi team,

We are using IMXRT1170 EVK board for our project and MCUxpresso IDE to develop the code.

Kindly provide the steps for the project creation in MCUxpresso IDE and also any project setting required to be set in-order to execute the code or binary built from the MCUxpresso project in the SDRAM of the imxrt1170 evk board.

标记 (3)
0 项奖励
回复
3 回复数

3,659 次查看
lpcxpresso_supp
NXP Employee
NXP Employee
0 项奖励
回复

3,645 次查看
Jeevan
Contributor IV

Hi @lpcxpresso_supp 

Thank you, team, it's a good document which you have shared to make the code boot from SDRAM.

Just had one small query, as the IMXRT1176 comes with 2 MB on-chip RAM, is the process mentioned in the section 14 of the "Using the MIMXRT1170-EVK and EVKB with MCUXpresso IDE" (RT1170_BriefOverview_v200.pdf) document same or any modifications need to be done.

0 项奖励
回复

3,625 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Thanks for sharing this detailed documentation, it's fantastic! For the IMXRT1176, the modifications for using the MCUXpresso IDE are the same as in the documentation. Just need to check "Link to RAM" and move the SDRAM to the first RAM location.

 

0 项奖励
回复