Controlling 7-segment displays with i2c drivers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Controlling 7-segment displays with i2c drivers

跳至解决方案
412 次查看
Transidico
Contributor III

Good morning,

I have a question. I am using the i2c pca9956btwy driver to control two 3-digit 7-segment displays. I am using the i2c peripheral in polling mode with the I2C_MasterTransferBlocking function. In the background, I have a kind of scheduler with systick that uses some interrupts as timers. The problem is that I change the text on the displays very often within the while(1) of the main, so I lose some interrupts. My question is: if I keep the i2c peripheral in polling mode with the blocking function when I wait for the end of a transfer, if the interrupt triggers, I won't miss it, correct? Do I execute the interrupt and then return to waiting for the end of the transfer? What causes me to lose interrupts are the continuous transfers via 12c, correct?

Thank you in advance for your reply.

Best regards

0 项奖励
回复
1 解答
331 次查看
Transidico
Contributor III

Good morning,

thank you for your reply,

but I have solved the problem by auto-incrementing the LEDs. Now the interrupts are almost never lost. I have implemented a way to avoid sending continuous transmissions to the display if they are the same as the previous status. Unfortunately, I read the status of the buttons with the pca9534d driver every 20 ms, and I don't know how to reduce the transmissions, which means that I lose some interrupts. I can't increase the reading time, otherwise the buttons would not be in real time. Perhaps I could solve this by setting different interrupt priorities?

Thank you again.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
391 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello

Yes, interrupts should still be executed. However, what might be causing you to miss some of them is the frequent I2C transfers you're performing. These can overload the CPU and delay the handling of interrupts, especially if you're using blocking calls.

By the way, what microcontroller are you using?

0 项奖励
回复
372 次查看
Transidico
Contributor III

Thank you for your reply.
I am using mcxc242 and pca9956btwy to control the displays. Regarding the driver, is there a single command that allows me to select the PWM intensity of each pin in sequence without having to send the command for each pin in sequence?
Thank you again.

Regards

0 项奖励
回复
347 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Please see the GRPPWM register (section 7.3.4 of the Datasheet)

https://www.nxp.com/docs/en/data-sheet/PCA9956B.pdf

0 项奖励
回复
332 次查看
Transidico
Contributor III

Good morning,

thank you for your reply,

but I have solved the problem by auto-incrementing the LEDs. Now the interrupts are almost never lost. I have implemented a way to avoid sending continuous transmissions to the display if they are the same as the previous status. Unfortunately, I read the status of the buttons with the pca9534d driver every 20 ms, and I don't know how to reduce the transmissions, which means that I lose some interrupts. I can't increase the reading time, otherwise the buttons would not be in real time. Perhaps I could solve this by setting different interrupt priorities?

Thank you again.

0 项奖励
回复