Configuring a new MCUXpresso Project driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring a new MCUXpresso Project driver

1,764 Views
anbui
Contributor II

Why are the drivers I select when setting up my project not pulled and put in the project?

Do I need to copy each one individually over?

or

Am I selecting a wrong option?

0 Kudos
Reply
1 Reply

1,659 Views
lpcxpresso_supp
NXP Employee
NXP Employee

When you click on the new project wizard's Finish button, all of the selected driver files should be copied into the project created in your workspace. There will be a number of folders created within the project, so make sure you check them all to see the driver files.

If you are still having problems, can you provide more details of what the project you create actually contains?

Note : For more details of creating projects, please check out the MCUXpresso IDE User Guide, supplied as part of the product install.

Regards,

MCUXpresso IDE Support

0 Kudos
Reply