Change CPU to LPC51U68JBD48 from LPC51U68JBD64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change CPU to LPC51U68JBD48 from LPC51U68JBD64

491 Views
BetoGreen
Contributor III

I have a LPC51U68JBD64 demo board and its SDK installed all working fine.

But our product uses LPC51U68JBD48. How do I change the CPU package to the 48pin?  The sdk shows 2 packages the D64 and D48.

I tried all sorts of things today including creating a new workspace and project but the configuration tool always comes up as LPC51U68JBD64.

I must be missing something....

 

 

0 Kudos
1 Reply

478 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello BetoGreen,

 

1) If you create new project, you can choose 48 pins as below:

Alice_Yang_0-1602473727706.png

 

2) If want to change under a demo project, change package as below:

 
 
 
 
 
 

Alice_Yang_0-1602474370879.png

 

Hope it helps,

Alice

 

 

 
 
 
 

 

 

 

 

0 Kudos