@Alice_Yang
Any idea what's causing this?
I've tried two different LPCXpresso54S018 boards, a Windows 11 desktop and Windows 11 laptop and two different Micro USB cables.
I've connected the USB directly to the PC and laptop, and from the laptop via an externally-powered USB hub and get the same results.
I tried running the software on Fedora 39, but it does not easily install so I've given up for now.
On one board I've tried LinkServer and J-Link firmware on the built-in debugger, and an external J-Link Plus Compact.
I plugged in a USB power meter while debugging with the J-Link Plus, and the power looks good. 5.0V and 0.1A idling, and 0.2A on the rare occasion it downloads and debugs freertos_hello correctly.
What else can I try?