I just downloaded gpio driver example to my OM13092 kit. While the Link probe is connected to it, it works fine, but it doesn't work when it runs stand alone. Is there a specific hardware setting to do it like a jumper or something like that?
Solved! Go to Solution.
Hi Marco,
You seem to have semihosting enabled for your project, please try disabling this option to the project properties:
When you import a project there is an option on the wizard where you chose to enable or disable this option:
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer
Do you download it to RAM or FLASH?
I also tried with Flash Programmer, but it didn't work.
Hi Marco,
You seem to have semihosting enabled for your project, please try disabling this option to the project properties:
When you import a project there is an option on the wizard where you chose to enable or disable this option:
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer
Hi, Carlos
Correct! It is working perfectly now!
Could you explain me what semihosting is?
Thanks!
Hi Marco,
Check out this Community document: https://community.nxp.com/docs/DOC-334074?sr=stream
-Anthony
Hi, Radomir!
Where do identify in MCUXpresso if I'm loading to RAM or Flash?