Hi,
I am using LPC 54018 IoT module along with OM 4006. I saw the schematic of OM 4006 board. It showed it has CAN bus ports. But I could not find any relevant sdk's to use it.
It would be great if someone could help me to use the SDK's.
Thanks and Regards
Niranjan
Hello Niranjan ravi,
Please use MCUXpresso SDK, there is CAN driver and demos.
You can download at https://mcuxpresso.nxp.com/en/select
There is CAN demo under drive_examples folder:
Hope it helps,
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you for your reply.
My bad, i was looking for flexcan. got it figured.
Thank you
Thanks and Regards
Niranjan