CAN MCUXpresso not communicate with CAN KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN MCUXpresso not communicate with CAN KDS

523件の閲覧回数
avppoian
Contributor I

There is a difference on the code of SDK MCUXpresso and the processor expert bean of KDS. It is not possible to communicate CAN with other microcontrollers and the other microcontroller NXP writing the code in KDS because a mask on frame.id. I tryed everything and it is impossible to communicate. From the side of MCUXpresso when you send it stays on while(!txComplete). I modified the timing bit calculation and not happens. I can communicate between two boards writing the software on both with MCUXpresso. There is a bug on MCUXpresso that is not possible to communicate with other microcontrollers. I think that is exclusive and you should write software and use only microcontrollers wrote with MCUXpresso only. I need help to now how to communicate with others microcontrollers and the same microcontroller wrote in KDS.

ラベル(1)
0 件の賞賛
1 返信

433件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

The case question have been replied on your salesforce case.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛