Build and re-flash while debugging

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Build and re-flash while debugging

1,171 次查看
bbenj
Contributor III

Hello,

I was wondering if it is possible to flash an MCU while running a debug session in MCUXpresso? Not having to stop the redlink server and restart a debug session every time I make a change would save me a lot of time, Eclipse is pretty slow...

I'm working with a i.MX RT 1021 & CMSIS-DAP, but I guess the option would work for any MCU?.

I searched the internet and Eclipse menus, but didn't find anything. I hope there's something I missed!

Thanks,

Best regards,

Benjamin

0 项奖励
回复
1 回复

1,101 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

MCUXpresso IDE does not support flash (re)programming while dealing with a live debug session. Flash is programmed only at the beginning of an actual debug session or as a completely separate action.

Greetings,
MCUXpresso IDE Support

0 项奖励
回复