I am trying to run the Beacon demo example on the KW45B41-EVK. After flashing pressing SW RST and ADV I still do not get the info in the IoT toolbox. Also there is nothing in the connected terminal. I tried with other BLE examples and the result is the same. If I just try regular examples like the shell example or blink led example they work perfectly. What can I possibly be doing wrong?
Hello @Yul81
Hope you are doing well.
Just to confirm, what SDK version are you using? Have you been able to successfully run any of the BLE example projects before?
It is necessary to work with the matching NBU image for the SDK version of the application you are working with. Prior to loading any wireless SDK example, please update your NBU image.
The Getting Started with the KW45B41Z Evaluation Kit describes the first steps to work with your device. Section 3.3 Updating NBU for Wireless Examples describes how to update the NBU using SPSDK command line tool (installation of SPSDK is described in Section 2.4). Please, make sure to have Python 3.7+ installed.
Please, follow the steps listed in the Getting Started and let me know your findings.
Regards,
Eduardo.
I followed the steps on the guide to install the SPSDK for Windows. I executed without issues steps 1 through 4, but for step 5 I got the following message: 'spsdk' is not recognized as an internal or external command,operable program or batch file.
Regardless I tried to update the NBU but after having the board set in ISP mode, if I executed the nxpdevscan command I got the same message as for when I executed the spsdk --help command.
'nxpdevscan' is not recognized as an internal or external command,
operable program or batch file.
What went wrong?
Also just to confirm ISP mode is when the RGB LED is set on blue right?
Hi,
Please, try the whole installation procedure again. If the you face the same issue, try the following (after performing step 4):
RGB LED on solid blue should indicate that your device is in ISP mode.
Regards,
Eduardo.