Hi friends,
I am currently working on a project using the following environment:
-NXP RT1060
-MCUXpresso IDE v11.7.1 [Build 9221] [2023-03-28]
-SDK_2.x_MIMXRT1060-EVKB
Initially, I used GUI-guider to design my user interface and exported the project to MCUXpresso for further design. However, I encountered a problem.
Now, I would like to add events to control component actions. Should I add event files in the source files or in the generated files or something else?
And what should I do first? I have limited knowledge of MCUXpresso IDE, but I have to use it for design.
I would greatly appreciate it if someone could lprovide guidance.