Adding Components to MQTT FreeRTOS DemoBreaks demo with SDK LWIP Overwrites

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding Components to MQTT FreeRTOS DemoBreaks demo with SDK LWIP Overwrites

543件の閲覧回数
stevenlutz
Contributor III

I have started with the MQTT FreeRTOS Demo on the MCXN947. The demo works fine, however when a component is added, eg, FlexCan. Then the components get updated including LWIP. 
LWIP is then broken with an error involving the functions for name reoslution. 

In order to move forward and I had to manually copy and include each additional component from another project in order to keep the original LWIP files in place. 

Please advise. Thank you

FRDM-MCXN947 

0 件の賞賛
返信
1 返信

516件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @stevenlutz 

How did you add Flexcan related component?

Will lwip still break when you manually add the relevant code?

BR

Harry

0 件の賞賛
返信