Yes, I know that case and has also referred to that on the other thread Debug problems on MIMXRT1050-EVK . I have reported the problem to Adaware (hopefully the mcuxpressoide.exe file gets through). Let us see if they can find out if it is a false positive or MCUXpresso is doing something suspicious, which it ought not to do. Anti virus programs must respond to suspicious behavior to be able to detect previously unknown viruses, but this also put some demands on the programmers, who must do everything by the book to prevent a false positive detection.
Since others - except for that thread - have not seen similar problems and we also have MCUXpresso running on a Windows 10 laptop with the same version of Adaware without any virus warnings, it is probably a false positive. Unfortunately, Adaware has no way to mark a given file as safe, so I would have to switch off the real time protection every time I would use MCUXpresso and this is an unacceptable solution, as it will also disable the real time protection for everything else running on the computer.