About new SDK wizard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About new SDK wizard

1,407 Views
ogawatakeshi
Contributor II

SDK 73.png

I would like to ask about Board SDK Wizard.

Are there any main usage and examples?

0 Kudos
Reply
5 Replies

1,221 Views
ogawatakeshi
Contributor II

Thank you for kindly mail.

Well noted.

I look forward to future development.

Best regard,

0 Kudos
Reply

1,221 Views
lpcxpresso_supp
NXP Employee
NXP Employee

The "Board SDK wizard" is functionality that we are trialing internally at present, rather than something intended for customer use at this stage. But basically its aim is to allow the generation of an "add-on" SDK package that provides information to the IDE on a customer / third party board by installing in combination with a standard SDK.

We'll be releasing more information/documentation on this functionality in due course. We strongly advise waiting until we do so before you investigate this functionality for yourself - as using it requires a very good level of understanding of how SDKs and the IDE interact.

Regards,

MCUXpresso IDE Support

1,221 Views
antonypace
Contributor II

I too am interested in this. I can see that the New Board SDK Wizard is present in the current MCUXpresso. It was a year since the original question, is there an update on this?

0 Kudos
Reply

1,221 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi OGAWA:

Please refer to the MCUXpresso_IDE_User_Guider.pdf.

Chapter 6, Creating New Projects using installed SDK part Support.

pastedImage_1.png

Regards

Daniel

0 Kudos
Reply

1,221 Views
ogawatakeshi
Contributor II

Hi Daniel.

Thanks for reply.

I'd like to know new board sdk creator.(not new project create.

Is it possible to (New/Board SDK Wizard create) new board SDK?

0 Kudos
Reply