最近在做基于LPC55S69的SD卡扩展,但是完全不知道怎么入手啊,由于LPC55S69又是一个比较新的单片机,所以也没找到相关的SD卡开发程序,请问大家有相关的资源吗?诚心求教怎么写SD卡的程序,还有,sdk的开发例程,可以用来参考写自己的SD卡程序吗?谢谢大家了!1
Hi 小白 张
There is SD card demo code under LPC55s69 SDK.
you need download 55s69 SDK from this url
Welcome | MCUXpresso SDK Builder
Then find demo code code from this path:
{LPCXpresso55S69 SDK folder}\boards\lpcxpresso55s69\driver_examples\sdcard
there is readme.txt under the project folder which tells how to use the demo code.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
--------------------------------------------------------------------------