MCUXpresso IDE v11.7.1 Now Available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso IDE v11.7.1 Now Available

MCUXpresso IDE v11.7.1 Now Available

We are pleased to announce that MCUXpresso IDE v11.7.1 (build 9221) is now available.

This is a maintenance release that builds upon the previous MCUXpresso IDE v11.7.0 release, and we recommend that all existing users download and install this new version.

 

Installer Downloads 

To download the installers for all platforms, please login to our download site via: 

 

Documentation 

Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from:

 

Notification of future releases 

To receive notifications about future releases, please follow: MCUXpresso IDE - Release History 

 

Summary of Changes - version 11.7.1 - March 2023

  • Upgraded: Newer SEGGER J-Link software (v7.86e).
  • Upgraded: Newer PEmicro plugin (v5.5.5).
  • Upgraded: Version v13.1 of MCUXpresso Config Tools.
  • Added support for LPC553x/S3x revision A1 device.
  • Added support for LPC860 revision A1 device.
  • Added support for KW45/K32W1 revision A2 device.
  • Improvement: [SWO] Added preference for SWO ITM rxBuffer reading timeout in Preferences -> MCUXpresso IDE -> SWO Trace -> ITM_RxBuffer send timeout. This is intended to allow timeout increase in case user determines the application is not able to consume full amount of (so it will appear to lose) data sent by host debugger with the current timeout settings.
  • Fixed: [Debug] Can't create a new launch configuration after using GUI Flash Tool on PEmicro.
  • Fixed: [X-KW45B41Z-EVK][MCU-Link] Debug error reported when using MCU-Link firmware 3.x.
  • Fixed: [Debug][PN7642] Update reset script to fix Restart behavior in the IDE (not fully performing reset on certain clocks / peripherals).
  • Fixed: [Energy Measurement][Power Profile] Trigger configuration is visible for LPC-Link2 probes.
  • Fixed: [SWO] Starting debug session with SWO counters or interrupts views opened results in error.

Known issues

  • Please follow the KnownIssues.txt file from installation layout for a detailed list.
  • Note. Additional issues that will be found post-release will be added in an online version also aiming to describe workarounds when available.
100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎04-02-2023 10:59 PM
更新者: