xxx_PDD.h for MCUxpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

xxx_PDD.h for MCUxpresso

610 次查看
seapon
Contributor I

I would like to re-develop old designed code which was made with processor expert on MCUxpresso.

This code referred to xxx_PDD.h,  I cannot get  any xxx_PDD.h for MCUxpresso. If input/output condition of each xxx_PDD is opened, I think I can make drivers for MCUexprsso.

0 项奖励
1 回复

554 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Masato Nishimoto ,

MCUXpresso IDE doesn't integrate Processor Expert in default.

You can refer to Erich's blog to add it:

MCUXpresso IDE: Installing Processor Expert into Eclipse Neon | MCU on Eclipse 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励