things that happen to start debugging RT1051

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

things that happen to start debugging RT1051

1,504件の閲覧回数
mastupristi
Senior Contributor I

When I launch the debug of an RT1051 from MCUXpresso on the debugger console there is this

[19-12-2018 03:55:15] Executing Server: /opt/SEGGER/JLink_V632h/JLinkGDBServerCLExe -nosilent -swoport 2332 -select USB=504400379  -telnetport 2333 -singlerun -endian little -noir -speed auto   -port 2331   -vd -device MIMXRT1051xxxxB -if SWD -halt -reportuseraction
SEGGER J-Link GDB Server V6.32h Command Line Version

JLinkARM.dll V6.32h (DLL compiled Jul  5 2018 18:14:58)

Command line: -nosilent -swoport 2332 -select USB=504400379 -telnetport 2333 -singlerun -endian little -noir -speed auto -port 2331 -vd -device MIMXRT1051xxxxB -if SWD -halt -reportuseraction
-----GDB Server start settings-----
GDBInit file:                  none
GDB Server Listening port:     2331
SWO raw output listening port: 2332
Terminal I/O port:             2333
Accept remote connection:      yes
Generate logfile:              off
Verify download:               on
Init regs on start:            off
Silent mode:                   off
Single run mode:               on
Target connection timeout:     0 ms
------J-Link related settings------
J-Link Host interface:         USB
J-Link script:                 none
J-Link settings file:          none
------Target related settings------
Target device:                 MIMXRT1051xxxxB
Target interface:              SWD
Target interface speed:        auto
Target endian:                 little

Connecting to J-Link...
J-Link is connected.
Device "MIMXRT1051XXXXB" selected.
Firmware: J-Link Ultra V4 compiled Oct 26 2018 12:04:46
Hardware: V4.00
S/N: 504400379
Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB
Checking target voltage...
Target voltage: 3.39 V
Listening on TCP/IP port 2331
Connecting to target...Found SW-DP with ID 0x0BD11477
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x04770041)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FD000
CPUID register: 0x411FC271. Implementer code: 0x41 (ARM)
Found Cortex-M7 r1p1, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
CoreSight components:
ROMTbl[0] @ E00FD000
ROMTbl[0][0]: E00FE000, CID: B105100D, PID: 000BB4C8 ROM Table
ROMTbl[1] @ E00FE000
ROMTbl[1][0]: E00FF000, CID: B105100D, PID: 000BB4C7 ROM Table
ROMTbl[2] @ E00FF000
ROMTbl[2][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7
ROMTbl[2][1]: E0001000, CID: B105E00D, PID: 000BB002 DWT
ROMTbl[2][2]: E0002000, CID: B105E00D, PID: 000BB00E FPB-M7
ROMTbl[2][3]: E0000000, CID: B105E00D, PID: 000BB001 ITM
ROMTbl[1][1]: E0041000, CID: B105900D, PID: 001BB975 ETM-M7
ROMTbl[1][2]: E0042000, CID: B105900D, PID: 004BB906 CTI
ROMTbl[0][1]: E0040000, CID: B105900D, PID: 000BB9A9 TPIU-M7
ROMTbl[0][2]: E0043000, CID: B105F00D, PID: 001BB101 TSG
Cache: Separate I- and D-cache.

I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way
D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
Found SW-DP with ID 0x0BD11477
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FD000
CPUID register: 0x411FC271. Implementer code: 0x41 (ARM)
Found Cortex-M7 r1p1, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
CoreSight components:
ROMTbl[0] @ E00FD000
ROMTbl[0][0]: E00FE000, CID: B105100D, PID: 000BB4C8 ROM Table
ROMTbl[1] @ E00FE000
ROMTbl[1][0]: E00FF000, CID: B105100D, PID: 000BB4C7 ROM Table
ROMTbl[2] @ E00FF000
ROMTbl[2][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7
ROMTbl[2][1]: E0001000, CID: B105E00D, PID: 000BB002 DWT
ROMTbl[2][2]: E0002000, CID: B105E00D, PID: 000BB00E FPB-M7
ROMTbl[2][3]: E0000000, CID: B105E00D, PID: 000BB001 ITM
ROMTbl[1][1]: E0041000, CID: B105900D, PID: 001BB975 ETM-M7
ROMTbl[1][2]: E0042000, CID: B105900D, PID: 004BB906 CTI
ROMTbl[0][1]: E0040000, CID: B105900D, PID: 000BB9A9 TPIU-M7
ROMTbl[0][2]: E0043000, CID: B105F00D, PID: 001BB101 TSG
Cache: Separate I- and D-cache.

I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way
D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
Connected to target
Waiting for GDB connection...Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0x00206742 (Data = 0x68139901)
Read 2 bytes @ address 0x00206742 (Data = 0x9901)
Received monitor command: reset
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
Resetting target
Downloading 8192 bytes @ address 0x60000000 - Verified OK
Downloading 584 bytes @ address 0x60002000 - Verified OK
Downloading 16104 bytes @ address 0x60002248 - Verified OK
Downloading 15840 bytes @ address 0x60006130 - Verified OK
Downloading 16096 bytes @ address 0x60009F10 - Verified OK
Downloading 3196 bytes @ address 0x6000DDF0 - Verified OK
Downloading 12 bytes @ address 0x6000EA6C - Verified OK
Downloading 72 bytes @ address 0x6000EA78 - Verified OK
Downloading 780 bytes @ address 0x6000EAC0 - Verified OK
J-Link: Flash download: Bank 0 @ 0x60000000: 1 range affected (65536 bytes)
J-Link: Flash download: Total time needed: 2.227s (Prepare: 0.092s, Compare: 0.551s, Erase: 0.173s, Program: 0.834s, Verify: 0.561s, Restore: 0.013s)
Writing register (PC = 0x60002054)
Read 4 bytes @ address 0x60002054 (Data = 0xF8DFB672)
Reading all registers
Read 4 bytes @ address 0x60002054 (Data = 0xF8DFB672)
Read 2 bytes @ address 0x60002054 (Data = 0xB672)
Received monitor command: exec SetRestartOnClose=1
Executed SetRestartOnClose=1
Setting breakpoint @ address 0x60002054, Size = 2, BPHandle = 0x0001
Starting target CPU...
...Breakpoint reached @ address 0x60002054
Reading all registers
Removing breakpoint @ address 0x60002054, Size = 2
Read 4 bytes @ address 0x60002054 (Data = 0xF8DFB672)
Reading 64 bytes @ address 0x600020C0
Reading 64 bytes @ address 0x60002040
Reading 64 bytes @ address 0x60002080‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

There are two things I want to understand.

  1. On lines 96 and 97 I find that two readings are requested at the same address (0x00206742) of 4 and 2 bytes.
    [...]
    Reading all registers
    Read 4 bytes @ address 0x00206742 (Data = 0x68139901)
    Read 2 bytes @ address 0x00206742 (Data = 0x9901)
    Received monitor command: reset
    [...]
    Addresses between 0x00200000 and 0x00217FFF are within the ROMCP (ROM Bootloader). This also includes the address 0x00206742.
    Why is the reading of a location inside the ROM Bootloader requested? Why is the reading requested with two different dimensions?
  2. After writing the flash, the program counter is written instead of issuing a reset.
    [...]
    J-Link: Flash download: Bank 0 @ 0x60000000: 1 range affected (65536 bytes)
    J-Link: Flash download: Total time needed: 2.227s (Prepare: 0.092s, Compare: 0.551s, Erase: 0.173s, Program: 0.834s, Verify: 0.561s, Restore: 0.013s)
    Writing register (PC = 0x60002054)
    Read 4 bytes @ address 0x60002054 (Data = 0xF8DFB672)
    Reading all registers
    Read 4 bytes @ address 0x60002054 (Data = 0xF8DFB672)
    Read 2 bytes @ address 0x60002054 (Data = 0xB672)
    Received monitor command: exec SetRestartOnClose=1
    Executed SetRestartOnClose=1
    Setting breakpoint @ address 0x60002054, Size = 2, BPHandle = 0x0001
    Starting target CPU...
    ...Breakpoint reached @ address 0x60002054
    [...]
    Doing so the ROM Bootloader will not run. So the FW is in a different situation than when the device is started without debugger (initialized peripheral, clocks activated, etc...)
    How can I force a reset instead of writing to the PC, so that the ROM Bootloader will run?

best regards

Max

0 件の賞賛
返信
1 返信

1,314件の閲覧回数
buckfobb
Contributor II

Regarding #2 above, I have this question too.

For example, even though the boot "program image" sets up the flexspi flash to operate as qspi (verified when powered-on without debugger attached it is operating as qspi via logic analyzer), when using the debugger to program and debug it leaves the flexspi in slow basic spi mode (verified via logic analyzer). Thus, when running code via debugger it is running very slow if doing XIP.

Similar issue for sdram. I know NXP provides the jlink script file to set up the sdram from debugger but this script seems to prevent the debugger being able to program the spi flash.

I have worked around the debugger-skips-bootrom issue by programming the flash via debugger, doing a hard reset, and making the debugger connect to running target. However, tedious and not ideal.

Suggestions for solution welcomed.

0 件の賞賛
返信