kw41z freertos SPI connection with RFID RC-522

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kw41z freertos SPI connection with RFID RC-522

675 Views
satsok_n
Contributor III

I am trying to connect via SPI the RFID RC-522 with the FRDM-KW41Z. I downloaded the IDE for my board. I am trying to connect it using the freeRtos examples. I am using the DSPI example. I connected PTA18 as SCK, PTA17 as MISO, PTA16 as MOSI, PTA19 as SS. Is there any library that can be used to control the RFID(The only one found was for Arduino)?  Any suggestions?

0 Kudos
1 Reply

458 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Kostas,

Unfortunately there isn't any library available for the RFID RC-522. You could try porting the arduino example to work with the FRDM-KW41Z in base of the example you already using.

Sorry for the inconveniences this may cause you.

Best Regards,

Alexis Andalon

0 Kudos