kw41z freertos SPI connection with RFID RC-522

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kw41z freertos SPI connection with RFID RC-522

878件の閲覧回数
satsok_n
Contributor III

I am trying to connect via SPI the RFID RC-522 with the FRDM-KW41Z. I downloaded the IDE for my board. I am trying to connect it using the freeRtos examples. I am using the DSPI example. I connected PTA18 as SCK, PTA17 as MISO, PTA16 as MOSI, PTA19 as SS. Is there any library that can be used to control the RFID(The only one found was for Arduino)?  Any suggestions?

0 件の賞賛
返信
1 返信

661件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Kostas,

Unfortunately there isn't any library available for the RFID RC-522. You could try porting the arduino example to work with the FRDM-KW41Z in base of the example you already using.

Sorry for the inconveniences this may cause you.

Best Regards,

Alexis Andalon

0 件の賞賛
返信