How configure USB1_PLL and 32KHz RTC to use temperature Monitor measurment on iMXRT1050 ?
Is there application example ?
Hi Michele Blanc,
Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the tempmon demo in the SDK library whose download link is below, please give a try.
MCUXpresso SDK|NXP
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jeremy,
Thank you for the answer. Can you tell me in which demo example in the Import SDK examples I will find the use of tempmon ?
Best regards
Michèle
De : jeremyzhou
Envoyé : jeudi 13 décembre 2018 12:20
À : BLANC Michelle <mblanc@centralp.fr>
Objet : Re: - Re: iMXRT1050 tempmon clock configuration
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: iMXRT1050 tempmon clock configuration
reply from jeremyzhou<https://community.nxp.com/people/jeremyzhou?et=watches.email.thread> in MCUXpresso Software and Tools - View the full discussion<https://community.nxp.com/message/1091267?commentID=1091267&et=watches.email.thread#comment-1091267>
Hi Michele Blanc,
Thanks for your reply.
After downloading the SDK library, then unzip it, you can find the tempmon demo resides in the ~\SDK_2.5.0_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you, I didn’t see the example, it was not in the SDK_2.4.0_EVKB-IMXRT1050. I found it in the new version.
Best regards
Michèle Blanc
De : jeremyzhou
Envoyé : lundi 17 décembre 2018 04:03
À : BLANC Michelle <mblanc@centralp.fr>
Objet : Re: - Re: iMXRT1050 tempmon clock configuration
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: iMXRT1050 tempmon clock configuration
reply from jeremyzhou<https://community.nxp.com/people/jeremyzhou?et=watches.email.thread> in MCUXpresso Software and Tools - View the full discussion<https://community.nxp.com/message/1092326?commentID=1092326&et=watches.email.thread#comment-1092326>