i.MX RT1064 not supported in ConfigTool Ver. 5.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX RT1064 not supported in ConfigTool Ver. 5.0

4,135 次查看
christianeugste
Contributor II

It looks like there is a difference in the available configurations between the ConfigTool Version 4.1 and the newest 5.0:

Actually should it not be possible to select the RT1064 in both version?
But it is missing in the selection at Version 5.0.

Any help appreciated.

标记 (1)
4 回复数

3,909 次查看
Lukas_Heczko
NXP Employee
NXP Employee

Hi Christian,

the RT1064 processor and board configurations are now available in MCUXpresso Config Tools v5 and MCUXpresso IDE 10.3. You will see them automatically when a new configuration in the tools is created.

We are sorry for the confusion and delay.

Regards,

Lukas

0 项奖励
回复

3,909 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi  Christian

Config Tool V5

pastedImage_2.png

Please refer to below link for details

MCUXpresso Config Tools v5 Now Available 

Regards

Daniel

0 项奖励
回复

3,909 次查看
christianeugste
Contributor II

Dear Daniel

Thank you for your reply, which confirms that imxrt1064 is not supported in V5.0.

But why?

On the office NXP website for i.MX RT1064 the MCUXpresso Config Tool is mentioned under “recommened Software & Tools”, so I don’t see any reason why it is not supported (anymore).

Best regards

Christian

Von: Daniel Chen <admin@community.nxp.com>

Gesendet: Mittwoch, 9. Januar 2019 08:51

An: Eugster Christian <Christian.Eugster@soudronic.com>

Betreff: You have been mentioned by Daniel Chen in Re: i.MX RT1064 not supported in ConfigTool Ver. 5.0 in NXP Community

NXP Community <https://emea01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.freescale.com%2Fresources%2Fstatics%2F1000%2F35400-NXP-Community-Email-banner-600x75.jpg&data=02%7C01%7Cchristian.eugster%40soudronic.com%7C37327701c2c64438fed808d676072dc9%7C2c1dce83d5b740b0b7f5819de9a7ff63%7C0%7C0%7C636826170543931867&sdata=nuTnvYjSztFyTnIHUKfKGdPZrMk7BssihZYkpEoz%2Fo8%3D&reserved=0>

You have been mentioned

by Daniel Chen<https://emea01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fpeople%2Fdanielchen%40fsl%3Fet%3Dnotification.mention&data=02%7C01%7Cchristian.eugster%40soudronic.com%7C37327701c2c64438fed808d676072dc9%7C2c1dce83d5b740b0b7f5819de9a7ff63%7C0%7C0%7C636826170543931867&sdata=g8EqQN6a85SwozYS0LnkNIQ9JerDWPwx1XCHXLLmgec%3D&reserved=0> in Re: i.MX RT1064 not supported in ConfigTool Ver. 5.0 in NXP Community - View Daniel Chen's reference to you<https://emea01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fmessage%2F1099027%3FcommentID%3D1099027%26et%3Dnotification.mention%23comment-1099027&data=02%7C01%7Cchristian.eugster%40soudronic.com%7C37327701c2c64438fed808d676072dc9%7C2c1dce83d5b740b0b7f5819de9a7ff63%7C0%7C0%7C636826170543931867&sdata=YFQBKRd1pOjpcVtotN2s44UBVqYQYGdwoeez1EFYoFE%3D&reserved=0>

0 项奖励
回复

3,909 次查看
petrstruzka
NXP Employee
NXP Employee

Hi, imxrt1064 is not supported in V5.0 yet, but it will be added soon. Sorry for inconvenience, we'll keep you informed.

Regards,

Petr