now i am trying to using the cyclone max debug the mpc5607b(100 LQFP),i use the PROGPPCNEXUS to connect the ic,but it notes "Can't communicate with the target processor!Please check your connections between the cable and the target and make sure the target has power"
the cyclone max use PORTB connect the jtagc。
Hello,
if you use PROGPPCNEXUS, please contact PeMicro support directly. It is their product, so they will provide better answer to you.
Regards,
Martin
I have Universal Multiliink, does it support to debug the mpc5607b?
发送自 Windows 10 版邮件<https://go.microsoft.com/fwlink/?LinkId=550986>应用
Hello,
yes, Universal Multilink supports mpc5607b.
Regards,
Martin
Hello,
first, I would like to ask, if you can write questions and answers in English, because out support is spread worldwide and official language is English.
About your question, which IDE you use? Cyclone MAX is standalone programmer, but without IDE, it cannot be used as a debugger.
If you want to use it as a debugger, please download CodeWarrior and set Cyclone in project debug settings. Please see the figure below:
Regards,
Martin