Hello.
I am currently using MCUXpresso version 11.5.0 because both versions 11.9.0 and 11.9.1 do not work properly in my environment.
I am currently inquiring about the issue, but it has not been resolved yet, so I am constantly looking for a solution.
Because of this situation, I want to downgrade my MCU-LINK-DEBUG-PROBE that I currently have.
I have three of them, but I updated two of them to V3.133 to use with MCUXpresso 11.9.0 or higher.
Therefore, only one can be used in version 11.5.0.
Also, the firmware version of the MCU-LINK-DEBUG-PROBE is currently V0.078.
So, I want to find the same version or a version that can be used in MCUXpresso version 11.5.0.
I am anxious because it is impossible to purchase additional ones now, and if they break down, I will not be able to work anymore.
I know how to upgrade using a script, but I am having difficulty finding the related firmware or a factory reset function to downgrade.
If anyone knows how or where to find the information, I would greatly appreciate the help.
Thank you.
解決済! 解決策の投稿を見る。
Hello @lehs
Sorry there isn't V0.078. How about MCULink_installer_2_207? I attach it for you.
You can install and update this firmware to test. Please contact us if still have any issue.
BR
Alice
Hello @Alice_Yang.
Thank you.
However, I cannot find the attached file in this content.
If you sent me the file via email, please let me know.
Since I haven't received any email, I need to contact the mail server administrator to check it.