Wrong pin export

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wrong pin export

950件の閲覧回数
s_schott
Contributor I

Hi there.

 

I am using  a LPC54618J512-TFBGA180 and Pins Tool V3.

 

I created a new empty config and saved it as a *.mex file.

Only with processor and package setting,

nothing else defined.

 

Then I exported a pin list (html) from this *.mex file

and found pin D7 = VDD2

 

But according to data sheet

"LPC546xx - Rev. 1.8 - 14 June 2017" - p.50

this is VSS5 instead.

 

Also pin H5 = VSS6 is exported as VD1_00.

 

 

Where's the mistake, please ?

0 件の賞賛
2 返答(返信)

720件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your sharing, this bug will be fixed on next release version MCUX_conf_tools_v_4.0_PRC2

Have a nice day!

Alice

0 件の賞賛

720件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello s. schott,

I haver reported it to MCUXpresso Configure tool expert team.

Sorry for the inconvenient to you.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛