Using MCUXpresso build project in Eclipse IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using MCUXpresso build project in Eclipse IDE

ソリューションへジャンプ
5,329件の閲覧回数
FAlexander
Contributor I

Hello,

This is first time I am working with NXP microcontrollers and MCUXpresso IDE, But all our projects till now are with Eclipse IDE. No we are planning to do the configuration part in MCUXpresso and still do the development and build in Eclipse IDE. I am using i.MX RT1010 MCU. 

I downloaded MCUXpresso SDK and have taken LED blinky example and able to build it in MCUXpresso, now if I want to take this same build project to Eclipse and build it will it be possible. Any suggestions or document would be helpful. Thanks in advance.

0 件の賞賛
返信
1 解決策
5,227件の閲覧回数
ErichStyger
Specialist I

I suggest you have a read at

Building a Triumvirate: From Eclipse CDT to CMake, CMD and Visual Studio Code | MCU on Eclipse

which shows how to use CMake both natively in Eclipse and outside, plus having access to all the MCUXpresso features like the configuration tools.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
5,228件の閲覧回数
ErichStyger
Specialist I

I suggest you have a read at

Building a Triumvirate: From Eclipse CDT to CMake, CMD and Visual Studio Code | MCU on Eclipse

which shows how to use CMake both natively in Eclipse and outside, plus having access to all the MCUXpresso features like the configuration tools.

I hope this helps,

Erich

0 件の賞賛
返信
5,178件の閲覧回数
FAlexander
Contributor I

 

Hello Enrich,

Am getting an error(please refer the attached image) while trying to build my project through command after following all the steps mentioned. Any guidance on this

0 件の賞賛
返信
5,174件の閲覧回数
ErichStyger
Specialist I

It seems you are using a different/wrong compiler. Either use the compiler which comes with the IDE or adjust the libraries you want to link with.

0 件の賞賛
返信
5,048件の閲覧回数
FAlexander
Contributor I

Hello Enrich,

Thank for the help. Now through CMake build am able to build in both MCUXpresso and Eclipse IDE but for debugging is there anyway I can use NXP LinkServer connection or it can be done only with Jlink?

0 件の賞賛
返信
5,038件の閲覧回数
ErichStyger
Specialist I

You can use and gdb server based debug probe, which includes the LinkServer which has added command line and gdb server capabilities recently, see https://mcuoneclipse.com/2023/05/14/linkserver-for-microcontrollers/

0 件の賞賛
返信
5,298件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, unfortunately, there is no information about the migration to Eclipse from NXP, but I found this thread maybe could help you.

Tutorial: Creating Bare-bare Embedded Projects with CMake, with Eclipse included | MCU on Eclipse

Best regards,
Pavel

 

0 件の賞賛
返信