Unable to compile RT1051 C++ project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to compile RT1051 C++ project

5,724 Views
mateuszpiesta
Contributor II

Hello,

Since few hours I'm struggling with compilation error of C++ project based on RT1051 uC. During my investigation I found that those two defines from fsl_clock.h are causing problems:

CCM_TUPLE and CCM_ANALOG_TUPLE

I'm using GNU Arm Embedded Toolchain Version 8-2018-q4-major and CMake, compilator spits those errors:

../bsp/drivers/fsl_clock.h:90:110: error: dereferencing a null pointer in '*0'
#define CCM_ANALOG_TUPLE(reg, shift) ((((uint32_t)(&((CCM_ANALOG_Type *)0U)->reg) & 0xFFFU) << 16U) | (shift))


../bsp/drivers/fsl_clock.h:90:110: error: enumerator value for 'kCLOCK_PllUsb2' is not an integer constant
#define CCM_ANALOG_TUPLE(reg, shift) ((((uint32_t)(&((CCM_ANALOG_Type *)0U)->reg) & 0xFFFU) << 16U) | (shift))

../bsp/drivers/fsl_clock.h:594:34: error: expression '0->CCM_Type::CCSR' has side-effects
((((uint32_t)(&((CCM_Type *)0U)->reg)) & 0xFFU) | ((shift) << 8U) | ((((mask) >> (shift)) & 0x1FFFU) << 13U) | \
((busyShift) << 26U))

It looks like g++ compiler is having some difficulties with compiling those macros. 

If I won't include "fsl_clock.h" compilation is working. There is no such problem when using gcc compiler.

Any ideas how to fix this issue ? I would be very grateful.

Best Regards

Mateusz Piesta

Tags (2)
12 Replies

5,259 Views
barrett_lowe
Contributor II

This issue can be seen here

5,259 Views
mateuszpiesta
Contributor II

Hi Kerry,

I've forgotten to mention that I've already tried MCUXpresso. C++ project generated by MCUXpresso is working flawlessly. I believe this is due to different version(probably older) of arm-gcc compiler. I didn't have any issues with this header using older versions of g++ compiler using custom CMake project.

Fortunately I was able to fix this issue. I had to modify those two macros, I used compiler built-in "offsetof" function to calculate structure offsets.

#define CCM_TUPLE(reg, shift, mask, busyShift) \
(((uint32_t)offsetof(CCM_Type,reg) & 0xFFU ) | ((shift) << 8U) | ((((mask) >> (shift)) & 0x1FFFU) << 13U) | \
((busyShift) << 26U))

 

#define CCM_ANALOG_TUPLE(reg, shift) ((((uint32_t)offsetof(CCM_ANALOG_Type,reg) & 0xFFFU) << 16U) | (shift))

After this modification my project is compiling fine without any problems. 

Maybe you should consider upgrading this defines ? This error was easily reproduced on different machines and under different OSes(Windows 10/7, ArchLinux).

Best regards

Mateusz Piesta

5,259 Views
anirudhan
Contributor II

Hi I am facing the same issue. I created a new C++ project and when I try to build I am getting the same errors as yours. The two macros in fsl_clock.h are creating problems. I am a beginner in embedded programming so Can you please detail out the method to fix this problem? kerryzhoubarrett.lowe@etcconnect.commateuszpiesta

0 Kudos
Reply

5,259 Views
Lukas_Heczko
NXP Employee
NXP Employee

Hi Anirudhan,

just to doublecheck, what SDK version do you use? I checked with the MCUXpresso SDK team and the problem with the macros should be resolved in SDK v2.6.0.

Regards,

Lukas

0 Kudos
Reply

5,259 Views
anirudhan
Contributor II

Hi Lukas,

I am working on the EVK-MiMXRT1050 board and the latest version of SDK for that board is 2.3. We are planning to move to the EVKB-MiMXRT1050 board which has the updated SDK 2.6.

0 Kudos
Reply

5,259 Views
anirudhan
Contributor II

Thanks a lot for your reply mateuszpiestabarrett.lowe@etcconnect.com. I have made the changes as Mateusz said, and it worked for me. 

0 Kudos
Reply

5,259 Views
barrett_lowe
Contributor II

For me, I just replaced the macros with the ones listed above or in the article that I linked. Kind of a hack but it worked...

5,259 Views
mateuszpiesta
Contributor II

Hi Anidudhan,

As I mentioned replace those two macros with :

#define CCM_TUPLE(reg, shift, mask, busyShift) \
(((uint32_t)offsetof(CCM_Type,reg) & 0xFFU ) | ((shift) << 8U) | ((((mask) >> (shift)) & 0x1FFFU) << 13U) | \
((busyShift) << 26U))

 

#define CCM_ANALOG_TUPLE(reg, shift) ((((uint32_t)offsetof(CCM_ANALOG_Type,reg) & 0xFFFU) << 16U) | (shift))

Also don't forget to add above those two defines: 

#include <stddef.h>

After those modifications project should compile. If you have any further questions/problems please let me know. 

I wonder why this was not included into the new SDK release. It is clear that newer versions of g++ have problems with old C style macros. 

I just want to add that it's been a while since I've made those changes and to this day everything seems to work as expected. I haven't encountered any problems so far.

Have a great day !

Mateusz Piesta

5,259 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mateusz Piesta,

    Thanks a lot for your updated information.

    After you modify it, do you also test the project function? Whether it works OK or not on your side?

    About your modification for C++, I will record it, thank you!

   


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,259 Views
mateuszpiesta
Contributor II

Hi Kerry,

We are using RT1050 in quite big and complex project which uses wide range of peripherals. After those changes everything seems to work as usual (we are in middle of converting some project modules to use C++ instead of C). Hence I believe it is pretty safe to say that those changes didn't break anything :smileyhappy:

Best regards

Mateusz Piesta

0 Kudos
Reply

5,259 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mateusz Piesta,

    Thanks a lot for your contribution!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,259 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mateusz Piesta,

       Actually, CCM_TUPLE and CCM_ANALOG_TUPLE just the simple shift and the or calculation.

      So, it should still in the compiler side.

     Do you mind to try the MCUXpresso IDE, whether it also have problems on your side.

     If after you tried the MCUXpresso IDE, it also have problems, please kindly let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply