I have a NXP board type FRDM-KL03Z with bootloader Version 1.11 and PEMicro FRDM-KL03Z Mass Storage/Debug App ver 1.18 installed in the board's auxiliary processor.
Using the ARM GCC toolchain and MCUXpresso SDK 2.3.1, I have successfully built the example "hello_world.elf" file.
I downloaded and installed the USB driver "Windows PEDrivers_install.exe" from http://www.pemicro.com/opensda/index.cfm
Windows 7 Device Manager is showing this under Ports as "OpenSDA - CDC Serial Port (COM4)"
I converted the .elf file to .srec file
(Didn't know how to do this in Windows so I temporarily transferred to a Linux computer and used the following command:
arm-none-eabi-objcopy -O srec hello_world.elf hello_world.srec
Not sure if this conversion step is necessary.)
I then copied "hello_world.srec" to the FRDM-KL03Z board on my Windows 7 pc.
In Windows, I set up a terminal session on PuTTY with serial port COM4, 9600 baud, 8 data bits, 1 stop bit (no Parity, no flow control) specified.
When I pressed the reset button on the the FRDM-KL03Z board, I expected to see "hello world" on the PuTTY screen. But there was no response.
Where have I gone wrong?
Solved! Go to Solution.
denbigh1974@gmx.net wrote:
Con Verse wrote:
You need to copy a binary file to the device, not an SREC file.
But if you are trying to develop an application, I suggest you use an IDE with a debugger, such as MCUXpresso, Keil etc.
Thank you for your reply.
I'm a confused beginner. According to the following webpage, if I'm using P&E Micro's debugging interface I should download the file as .s19 or .srec, using OpenSDA v1:
OpenSDA Serial and Debug Adapter | NXP
At the moment, I'm not trying to develop an application. I just wish to establish that I can transfer a .srec file and get the KL03Z to operate
To answer my own question, I found that I had to transfer the file in .srec format from the p.c. to the board and then disconnect/reconnect the board's USB link
Con Verse wrote:
You need to copy a binary file to the device, not an SREC file.
But if you are trying to develop an application, I suggest you use an IDE with a debugger, such as MCUXpresso, Keil etc.
Thank you for your reply.
I'm a confused beginner. According to the following webpage, if I'm using P&E Micro's debugging interface I should download the file as .s19 or .srec, using OpenSDA v1:
OpenSDA Serial and Debug Adapter | NXP
At the moment, I'm not trying to develop an application. I just wish to establish that I can transfer a .srec file and get the KL03Z to operate
denbigh1974@gmx.net wrote:
Con Verse wrote:
You need to copy a binary file to the device, not an SREC file.
But if you are trying to develop an application, I suggest you use an IDE with a debugger, such as MCUXpresso, Keil etc.
Thank you for your reply.
I'm a confused beginner. According to the following webpage, if I'm using P&E Micro's debugging interface I should download the file as .s19 or .srec, using OpenSDA v1:
OpenSDA Serial and Debug Adapter | NXP
At the moment, I'm not trying to develop an application. I just wish to establish that I can transfer a .srec file and get the KL03Z to operate
To answer my own question, I found that I had to transfer the file in .srec format from the p.c. to the board and then disconnect/reconnect the board's USB link
You need to copy a binary file to the device, not an SREC file.
But if you are trying to develop an application, I suggest you use an IDE with a debugger, such as MCUXpresso, Keil etc.