The system cannot find the file specified.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The system cannot find the file specified.

跳至解决方案
3,352 次查看
talhamir49
Contributor III

Hi 

I'm using JN5189 Development kit. I'm Trying to run JN-AN1246 but getting this Error

"Compiling ../../../LTOSensor/Source/app_main.c into ../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/app_main.o...
../../../../../MCUXpressoIDE_11.3.0_5222/ide/tools/bin/arm-none-eabi-gcc -c -o ../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/app_main.o -DSINGLE_CHANNEL=0 -DSLEEP_ENABLE -DOM15081 -DOM15081R2 -DLTOSensor -DBUTTON_MAP_OM15081 -DEZ_MODE_INITIATOR -DEZ_ENABLE_GROUP -DAPP_NTAG_ICODE -DgClkUseFro32K=1 -DgPWR_UseAlgoTimeBaseDriftCompensate=1 -DgClkRecalFro32K=0 -DAPP_LOW_POWER_API -DUART=USART0 -DDBG_ENABLE -DPRINTF_ADVANCED_ENABLE -DUART_BAUD_RATE=115200 -DDEBUG_APP_BUTTON -DDEBUG_START_UP -DDEBUG_SENSOR_TASK -DDEBUG_SENSOR_STATE -DDEBUG_SLEEP_HANDLER -DDEBUG_PROCESS_BUTTONS -DDEBUG_ZCL_PROCESSING -DDEBUG_NWK_EVENT_HANDLER -DDEBUG_APP_NTAG -DDEBUG_EVENT_HANDLER -DDEBUG_POWER_ON_COUNTER -DDEBUG_PIR_EVENTS -DLTOSensor -DPIR_TYPE_OPEN_COLLECTOR -DJN518x=5189 -DJN5189=5189 -DJENNIC_CHIP_NAME=_JN5189 -DJENNIC_CHIP_FAMILY_NAME=_JN518x -D__JN518X__ -DCPU_JN518X -std=gnu99 -DCORE_M4 -D__CODE_RED -fno-common -fmessage-length=0 -fno-builtin -mcpu=cortex-m4 -mthumb -fomit-frame-pointer -Os -fshort-enums -Wall -Wpacked -fdata-sections -ffunction-sections -DWATCHDOG_ALLOWED -fno-lto -DLITTLE_ENDIAN_PROCESSOR -DJENNIC_HW_BBC_RXINCCA=1 -DJENNIC_HW_BBC_DMA=1 -DJENNIC_HW_BBC_ISA=0 -DJENNIC_SW_EXTERNAL_FLASH=0 -DUART_BACKWARDS_COMPATIBLE_API=1 -DRXPOWERADJUST_SUPPORT -I../board -I../../../../../SDKPackages/JN5189DK6/CMSIS/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/components/serial_manager -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/devices -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/debug_console -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/str -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/uMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/mMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/XCVR/DK6 -DJENNIC_CHIP=JN5189 -DJENNIC_CHIP_JN5189 -DJENNIC_CHIP_FAMILY=JN518x -DJENNIC_CHIP_FAMILY_JN518x -DJENNIC_STACK_ZCL -DJENNIC_MAC_MiniMacShim -Wall -Wunreachable-code -DEMBEDDED -DosNumberOfSemaphores=0 -DosNumberOfMutexes=0 -DosNumberOfMessageQs=0 -DosNumberOfMessages=0 -DosNumberOfEvents=0 -DgMainThreadStackSize_c=0 -DgMainThreadPriority_c=0 -DgTaskMultipleInstancesManagement_c=0 -DFSL_OSA_BM_TIMER_CONFIG=FSL_OSA_BM_TIMER_SYSTICK -DDBG_ENABLE -DDEBUG_ENABLE -DENABLE_RAM_VECTOR_TABLE -DSDK_DEVICE_FAMILY=JN5189 -DgPWRM_Support=1 -DgSupportBle=0 -DcPWR_FullPowerDownMode=1 -DZIGBEE_USE_FRAMEWORK=1 -DPDM_USER_SUPPLIED_ID -DPDM_NO_RTOS -DZPS_APL_OPT_SINGLE_INSTANCE -DOTA_NO_CERTIFICATE -DPLME_SAP -DZBPRO_DEVICE_TYPE_ZED -DBDB_SUPPORT_NWK_STEERING -DBDB_SUPPORT_FIND_AND_BIND_INITIATOR -DBDB_SUPPORT_OOBC -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/SerialMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSNWK/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSTSV/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZigbeeCommon/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSAPL/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PWRM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDUM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Lists -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DBG/Include -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugExceptionHandlers_jn518x/src/../inc -I/../Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugFifo/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OSAbstraction/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/FunctionLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/SecLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/RNG/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/MemManager/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Messaging/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OtaSupport/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/TimersManager/Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/External/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface/ -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/components/serial_manager/ -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/LowPower/Source/jn5189dk6/../../Interface/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/GPIO -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/MeasurementAndSensing/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Lighting/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/HVAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Closures/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SecurityAndSafety/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SmartEnergy/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/OTA/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Commissioning/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/ApplianceManagement/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/GreenPower/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/Generic/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZLO/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/NwkSteering -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/FindAndBind -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/OutOfBand -I../../../LTOSensor/Source -I../../../Common/Source -I../../../Common/Source/board -I../../../LTOSensor/Source/PIR -I../../../NFC/Include ../../../LTOSensor/Source/app_main.c -MD -MF ../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/app_main.d -MP
process_begin: CreateProcess(NULL, ../../../../../MCUXpressoIDE_11.3.0_5222/ide/tools/bin/arm-none-eabi-gcc -c -o ../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/app_main.o -DSINGLE_CHANNEL=0 -DSLEEP_ENABLE -DOM15081 -DOM15081R2 -DLTOSensor -DBUTTON_MAP_OM15081 -DEZ_MODE_INITIATOR -DEZ_ENABLE_GROUP -DAPP_NTAG_ICODE -DgClkUseFro32K=1 -DgPWR_UseAlgoTimeBaseDriftCompensate=1 -DgClkRecalFro32K=0 -DAPP_LOW_POWER_API -DUART=USART0 -DDBG_ENABLE -DPRINTF_ADVANCED_ENABLE -DUART_BAUD_RATE=115200 -DDEBUG_APP_BUTTON -DDEBUG_START_UP -DDEBUG_SENSOR_TASK -DDEBUG_SENSOR_STATE -DDEBUG_SLEEP_HANDLER -DDEBUG_PROCESS_BUTTONS -DDEBUG_ZCL_PROCESSING -DDEBUG_NWK_EVENT_HANDLER -DDEBUG_APP_NTAG -DDEBUG_EVENT_HANDLER -DDEBUG_POWER_ON_COUNTER -DDEBUG_PIR_EVENTS -DLTOSensor -DPIR_TYPE_OPEN_COLLECTOR -DJN518x=5189 -DJN5189=5189 -DJENNIC_CHIP_NAME=_JN5189 -DJENNIC_CHIP_FAMILY_NAME=_JN518x -D__JN518X__ -DCPU_JN518X -std=gnu99 -DCORE_M4 -D__CODE_RED -fno-common -fmessage-length=0 -fno-builtin -mcpu=cortex-m4 -mthumb -fomit-frame-pointer -Os -fshort-enums -Wall -Wpacked -fdata-sections -ffunction-sections -DWATCHDOG_ALLOWED -fno-lto -DLITTLE_ENDIAN_PROCESSOR -DJENNIC_HW_BBC_RXINCCA=1 -DJENNIC_HW_BBC_DMA=1 -DJENNIC_HW_BBC_ISA=0 -DJENNIC_SW_EXTERNAL_FLASH=0 -DUART_BACKWARDS_COMPATIBLE_API=1 -DRXPOWERADJUST_SUPPORT -I../board -I../../../../../SDKPackages/JN5189DK6/CMSIS/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/components/serial_manager -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/devices -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/debug_console -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/str -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/uMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/mMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/XCVR/DK6 -DJENNIC_CHIP=JN5189 -DJENNIC_CHIP_JN5189 -DJENNIC_CHIP_FAMILY=JN518x -DJENNIC_CHIP_FAMILY_JN518x -DJENNIC_STACK_ZCL -DJENNIC_MAC_MiniMacShim -Wall -Wunreachable-code -DEMBEDDED -DosNumberOfSemaphores=0 -DosNumberOfMutexes=0 -DosNumberOfMessageQs=0 -DosNumberOfMessages=0 -DosNumberOfEvents=0 -DgMainThreadStackSize_c=0 -DgMainThreadPriority_c=0 -DgTaskMultipleInstancesManagement_c=0 -DFSL_OSA_BM_TIMER_CONFIG=FSL_OSA_BM_TIMER_SYSTICK -DDBG_ENABLE -DDEBUG_ENABLE -DENABLE_RAM_VECTOR_TABLE -DSDK_DEVICE_FAMILY=JN5189 -DgPWRM_Support=1 -DgSupportBle=0 -DcPWR_FullPowerDownMode=1 -DZIGBEE_USE_FRAMEWORK=1 -DPDM_USER_SUPPLIED_ID -DPDM_NO_RTOS -DZPS_APL_OPT_SINGLE_INSTANCE -DOTA_NO_CERTIFICATE -DPLME_SAP -DZBPRO_DEVICE_TYPE_ZED -DBDB_SUPPORT_NWK_STEERING -DBDB_SUPPORT_FIND_AND_BIND_INITIATOR -DBDB_SUPPORT_OOBC -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/SerialMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSNWK/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSTSV/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZigbeeCommon/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSAPL/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PWRM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDUM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Lists -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DBG/Include -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugExceptionHandlers_jn518x/src/../inc -I/../Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugFifo/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OSAbstraction/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/FunctionLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/SecLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/RNG/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/MemManager/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Messaging/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OtaSupport/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/TimersManager/Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/External/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface/ -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/components/serial_manager/ -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/LowPower/Source/jn5189dk6/../../Interface/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/GPIO -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/MeasurementAndSensing/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Lighting/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/HVAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Closures/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SecurityAndSafety/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SmartEnergy/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/OTA/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Commissioning/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/ApplianceManagement/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/GreenPower/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/Generic/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZLO/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/NwkSteering -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/FindAndBind -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/OutOfBand -I../../../LTOSensor/Source -I../../../Common/Source -I../../../Common/Source/board -I../../../LTOSensor/Source/PIR -I../../../NFC/Include ../../../LTOSensor/Source/app_main.c -MD -MF ../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/app_main.d -MP, ...) failed.
make (e=2): The system cannot find the file specified."

 

Followed JN-AN1260 Document.

0 项奖励
1 解答
3,308 次查看
talhamir49
Contributor III

Figured out the problem

problem was of Tool chain location in makefile.

changed TOOLCHAIN_DIR_PATH = ../../../../../MCUXpressoIDE_11.3.0_5737/ide/tools

to 

TOOLCHAIN_DIR_PATH = ../../../../../MCUXpressoIDE_11.4.0_6237/ide/tools.

 

在原帖中查看解决方案

0 项奖励
9 回复数
3,343 次查看
ErichStyger
Senior Contributor V

To confirm what @converse said: your command line is definitely >8k, so you need to shorten it.

What you can do is to use the 'subst' command and create a virtual drive which results in shorter command line length.

0 项奖励
3,333 次查看
talhamir49
Contributor III

Hi @ErichStyger 

Thanks for your reply.

I'm new here and I didn't  get what you said. Can you please Explain it ?

"What you can do is to use the 'subst' command and create a virtual drive which results in shorter command line length.

0 项奖励
3,327 次查看
ErichStyger
Senior Contributor V

subst is a windows command (google for it).

As for the command line length: check https://docs.microsoft.com/en-us/windows/win32/fileio/maximum-file-path-limitation?tabs=cmd

There is a registry key you could use.

I hope this helps,

Erich

0 项奖励
3,321 次查看
talhamir49
Contributor III

Its not a problem of path character size all the paths are set in makefile of example and all the locations are set according to the Document. Im also running JN5169 Example on beyond studio with greater path character  size and its work.

0 项奖励
3,314 次查看
converse
Senior Contributor V

Your path length is too long. You can choose to believe it, or not, that is up to you. Good luck in finding your own solution.

0 项奖励
3,316 次查看
talhamir49
Contributor III

I posted the whole compiling stuff but single file path is

"../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/SerialMAC/Include"

and its not out of limit. even as suggested to short the path length I tried that too with subst command. 

0 项奖励
3,309 次查看
talhamir49
Contributor III

Figured out the problem

problem was of Tool chain location in makefile.

changed TOOLCHAIN_DIR_PATH = ../../../../../MCUXpressoIDE_11.3.0_5737/ide/tools

to 

TOOLCHAIN_DIR_PATH = ../../../../../MCUXpressoIDE_11.4.0_6237/ide/tools.

 

0 项奖励
3,350 次查看
converse
Senior Contributor V

Windows is limited to a command line length of 8k characters - which yours seems to exceed. This is a Windows limitation and not MCUXpresso. You need to shorten the names of your directories...

3,336 次查看
talhamir49
Contributor III

hi @converse  Thanks for your reply.

But I don't think that problem lies in the length of 8k characters as I followed the the provided Document JN-AN1260 to use JN-AN-1246. All the directories names are already set in SDK and example code and locations of IDE SDK and Workspace are set according to the document.

0 项奖励