The system cannot find the file specified.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The system cannot find the file specified.

Jump to solution
5,954 Views
talhamir49
Contributor III

Hi 

I'm using JN5189 Development kit. I'm Trying to run JN-AN1246 but getting this Error

"Compiling ../../../LTOSensor/Source/app_main.c into ../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/app_main.o...
../../../../../MCUXpressoIDE_11.3.0_5222/ide/tools/bin/arm-none-eabi-gcc -c -o ../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/app_main.o -DSINGLE_CHANNEL=0 -DSLEEP_ENABLE -DOM15081 -DOM15081R2 -DLTOSensor -DBUTTON_MAP_OM15081 -DEZ_MODE_INITIATOR -DEZ_ENABLE_GROUP -DAPP_NTAG_ICODE -DgClkUseFro32K=1 -DgPWR_UseAlgoTimeBaseDriftCompensate=1 -DgClkRecalFro32K=0 -DAPP_LOW_POWER_API -DUART=USART0 -DDBG_ENABLE -DPRINTF_ADVANCED_ENABLE -DUART_BAUD_RATE=115200 -DDEBUG_APP_BUTTON -DDEBUG_START_UP -DDEBUG_SENSOR_TASK -DDEBUG_SENSOR_STATE -DDEBUG_SLEEP_HANDLER -DDEBUG_PROCESS_BUTTONS -DDEBUG_ZCL_PROCESSING -DDEBUG_NWK_EVENT_HANDLER -DDEBUG_APP_NTAG -DDEBUG_EVENT_HANDLER -DDEBUG_POWER_ON_COUNTER -DDEBUG_PIR_EVENTS -DLTOSensor -DPIR_TYPE_OPEN_COLLECTOR -DJN518x=5189 -DJN5189=5189 -DJENNIC_CHIP_NAME=_JN5189 -DJENNIC_CHIP_FAMILY_NAME=_JN518x -D__JN518X__ -DCPU_JN518X -std=gnu99 -DCORE_M4 -D__CODE_RED -fno-common -fmessage-length=0 -fno-builtin -mcpu=cortex-m4 -mthumb -fomit-frame-pointer -Os -fshort-enums -Wall -Wpacked -fdata-sections -ffunction-sections -DWATCHDOG_ALLOWED -fno-lto -DLITTLE_ENDIAN_PROCESSOR -DJENNIC_HW_BBC_RXINCCA=1 -DJENNIC_HW_BBC_DMA=1 -DJENNIC_HW_BBC_ISA=0 -DJENNIC_SW_EXTERNAL_FLASH=0 -DUART_BACKWARDS_COMPATIBLE_API=1 -DRXPOWERADJUST_SUPPORT -I../board -I../../../../../SDKPackages/JN5189DK6/CMSIS/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/components/serial_manager -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/devices -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/debug_console -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/str -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/uMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/mMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/XCVR/DK6 -DJENNIC_CHIP=JN5189 -DJENNIC_CHIP_JN5189 -DJENNIC_CHIP_FAMILY=JN518x -DJENNIC_CHIP_FAMILY_JN518x -DJENNIC_STACK_ZCL -DJENNIC_MAC_MiniMacShim -Wall -Wunreachable-code -DEMBEDDED -DosNumberOfSemaphores=0 -DosNumberOfMutexes=0 -DosNumberOfMessageQs=0 -DosNumberOfMessages=0 -DosNumberOfEvents=0 -DgMainThreadStackSize_c=0 -DgMainThreadPriority_c=0 -DgTaskMultipleInstancesManagement_c=0 -DFSL_OSA_BM_TIMER_CONFIG=FSL_OSA_BM_TIMER_SYSTICK -DDBG_ENABLE -DDEBUG_ENABLE -DENABLE_RAM_VECTOR_TABLE -DSDK_DEVICE_FAMILY=JN5189 -DgPWRM_Support=1 -DgSupportBle=0 -DcPWR_FullPowerDownMode=1 -DZIGBEE_USE_FRAMEWORK=1 -DPDM_USER_SUPPLIED_ID -DPDM_NO_RTOS -DZPS_APL_OPT_SINGLE_INSTANCE -DOTA_NO_CERTIFICATE -DPLME_SAP -DZBPRO_DEVICE_TYPE_ZED -DBDB_SUPPORT_NWK_STEERING -DBDB_SUPPORT_FIND_AND_BIND_INITIATOR -DBDB_SUPPORT_OOBC -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/SerialMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSNWK/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSTSV/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZigbeeCommon/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSAPL/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PWRM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDUM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Lists -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DBG/Include -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugExceptionHandlers_jn518x/src/../inc -I/../Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugFifo/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OSAbstraction/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/FunctionLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/SecLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/RNG/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/MemManager/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Messaging/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OtaSupport/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/TimersManager/Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/External/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface/ -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/components/serial_manager/ -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/LowPower/Source/jn5189dk6/../../Interface/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/GPIO -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/MeasurementAndSensing/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Lighting/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/HVAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Closures/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SecurityAndSafety/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SmartEnergy/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/OTA/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Commissioning/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/ApplianceManagement/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/GreenPower/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/Generic/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZLO/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/NwkSteering -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/FindAndBind -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/OutOfBand -I../../../LTOSensor/Source -I../../../Common/Source -I../../../Common/Source/board -I../../../LTOSensor/Source/PIR -I../../../NFC/Include ../../../LTOSensor/Source/app_main.c -MD -MF ../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/app_main.d -MP
process_begin: CreateProcess(NULL, ../../../../../MCUXpressoIDE_11.3.0_5222/ide/tools/bin/arm-none-eabi-gcc -c -o ../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/app_main.o -DSINGLE_CHANNEL=0 -DSLEEP_ENABLE -DOM15081 -DOM15081R2 -DLTOSensor -DBUTTON_MAP_OM15081 -DEZ_MODE_INITIATOR -DEZ_ENABLE_GROUP -DAPP_NTAG_ICODE -DgClkUseFro32K=1 -DgPWR_UseAlgoTimeBaseDriftCompensate=1 -DgClkRecalFro32K=0 -DAPP_LOW_POWER_API -DUART=USART0 -DDBG_ENABLE -DPRINTF_ADVANCED_ENABLE -DUART_BAUD_RATE=115200 -DDEBUG_APP_BUTTON -DDEBUG_START_UP -DDEBUG_SENSOR_TASK -DDEBUG_SENSOR_STATE -DDEBUG_SLEEP_HANDLER -DDEBUG_PROCESS_BUTTONS -DDEBUG_ZCL_PROCESSING -DDEBUG_NWK_EVENT_HANDLER -DDEBUG_APP_NTAG -DDEBUG_EVENT_HANDLER -DDEBUG_POWER_ON_COUNTER -DDEBUG_PIR_EVENTS -DLTOSensor -DPIR_TYPE_OPEN_COLLECTOR -DJN518x=5189 -DJN5189=5189 -DJENNIC_CHIP_NAME=_JN5189 -DJENNIC_CHIP_FAMILY_NAME=_JN518x -D__JN518X__ -DCPU_JN518X -std=gnu99 -DCORE_M4 -D__CODE_RED -fno-common -fmessage-length=0 -fno-builtin -mcpu=cortex-m4 -mthumb -fomit-frame-pointer -Os -fshort-enums -Wall -Wpacked -fdata-sections -ffunction-sections -DWATCHDOG_ALLOWED -fno-lto -DLITTLE_ENDIAN_PROCESSOR -DJENNIC_HW_BBC_RXINCCA=1 -DJENNIC_HW_BBC_DMA=1 -DJENNIC_HW_BBC_ISA=0 -DJENNIC_SW_EXTERNAL_FLASH=0 -DUART_BACKWARDS_COMPATIBLE_API=1 -DRXPOWERADJUST_SUPPORT -I../board -I../../../../../SDKPackages/JN5189DK6/CMSIS/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/components/serial_manager -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/devices -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/debug_console -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/str -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/uMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/mMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/XCVR/DK6 -DJENNIC_CHIP=JN5189 -DJENNIC_CHIP_JN5189 -DJENNIC_CHIP_FAMILY=JN518x -DJENNIC_CHIP_FAMILY_JN518x -DJENNIC_STACK_ZCL -DJENNIC_MAC_MiniMacShim -Wall -Wunreachable-code -DEMBEDDED -DosNumberOfSemaphores=0 -DosNumberOfMutexes=0 -DosNumberOfMessageQs=0 -DosNumberOfMessages=0 -DosNumberOfEvents=0 -DgMainThreadStackSize_c=0 -DgMainThreadPriority_c=0 -DgTaskMultipleInstancesManagement_c=0 -DFSL_OSA_BM_TIMER_CONFIG=FSL_OSA_BM_TIMER_SYSTICK -DDBG_ENABLE -DDEBUG_ENABLE -DENABLE_RAM_VECTOR_TABLE -DSDK_DEVICE_FAMILY=JN5189 -DgPWRM_Support=1 -DgSupportBle=0 -DcPWR_FullPowerDownMode=1 -DZIGBEE_USE_FRAMEWORK=1 -DPDM_USER_SUPPLIED_ID -DPDM_NO_RTOS -DZPS_APL_OPT_SINGLE_INSTANCE -DOTA_NO_CERTIFICATE -DPLME_SAP -DZBPRO_DEVICE_TYPE_ZED -DBDB_SUPPORT_NWK_STEERING -DBDB_SUPPORT_FIND_AND_BIND_INITIATOR -DBDB_SUPPORT_OOBC -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/SerialMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSNWK/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSTSV/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZigbeeCommon/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSAPL/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PWRM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDUM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Lists -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DBG/Include -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugExceptionHandlers_jn518x/src/../inc -I/../Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugFifo/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OSAbstraction/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/FunctionLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/SecLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/RNG/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/MemManager/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Messaging/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OtaSupport/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/TimersManager/Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/External/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface/ -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/components/serial_manager/ -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/LowPower/Source/jn5189dk6/../../Interface/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/GPIO -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/MeasurementAndSensing/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Lighting/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/HVAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Closures/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SecurityAndSafety/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SmartEnergy/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/OTA/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Commissioning/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/ApplianceManagement/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/GreenPower/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/Generic/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZLO/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/NwkSteering -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/FindAndBind -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/OutOfBand -I../../../LTOSensor/Source -I../../../Common/Source -I../../../Common/Source/board -I../../../LTOSensor/Source/PIR -I../../../NFC/Include ../../../LTOSensor/Source/app_main.c -MD -MF ../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/../../../Binaries/LTOSensor_NtagIcode_OM15081R2/obj/app_main.d -MP, ...) failed.
make (e=2): The system cannot find the file specified."

 

Followed JN-AN1260 Document.

0 Kudos
Reply
1 Solution
5,910 Views
talhamir49
Contributor III

Figured out the problem

problem was of Tool chain location in makefile.

changed TOOLCHAIN_DIR_PATH = ../../../../../MCUXpressoIDE_11.3.0_5737/ide/tools

to 

TOOLCHAIN_DIR_PATH = ../../../../../MCUXpressoIDE_11.4.0_6237/ide/tools.

 

View solution in original post

0 Kudos
Reply
9 Replies
5,945 Views
ErichStyger
Specialist I

To confirm what @converse said: your command line is definitely >8k, so you need to shorten it.

What you can do is to use the 'subst' command and create a virtual drive which results in shorter command line length.

0 Kudos
Reply
5,935 Views
talhamir49
Contributor III

Hi @ErichStyger 

Thanks for your reply.

I'm new here and I didn't  get what you said. Can you please Explain it ?

"What you can do is to use the 'subst' command and create a virtual drive which results in shorter command line length.

0 Kudos
Reply
5,929 Views
ErichStyger
Specialist I

subst is a windows command (google for it).

As for the command line length: check https://docs.microsoft.com/en-us/windows/win32/fileio/maximum-file-path-limitation?tabs=cmd

There is a registry key you could use.

I hope this helps,

Erich

0 Kudos
Reply
5,923 Views
talhamir49
Contributor III

Its not a problem of path character size all the paths are set in makefile of example and all the locations are set according to the Document. Im also running JN5169 Example on beyond studio with greater path character  size and its work.

0 Kudos
Reply
5,916 Views
converse
Senior Contributor V

Your path length is too long. You can choose to believe it, or not, that is up to you. Good luck in finding your own solution.

0 Kudos
Reply
5,918 Views
talhamir49
Contributor III

I posted the whole compiling stuff but single file path is

"../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/SerialMAC/Include"

and its not out of limit. even as suggested to short the path length I tried that too with subst command. 

0 Kudos
Reply
5,911 Views
talhamir49
Contributor III

Figured out the problem

problem was of Tool chain location in makefile.

changed TOOLCHAIN_DIR_PATH = ../../../../../MCUXpressoIDE_11.3.0_5737/ide/tools

to 

TOOLCHAIN_DIR_PATH = ../../../../../MCUXpressoIDE_11.4.0_6237/ide/tools.

 

0 Kudos
Reply
5,952 Views
converse
Senior Contributor V

Windows is limited to a command line length of 8k characters - which yours seems to exceed. This is a Windows limitation and not MCUXpresso. You need to shorten the names of your directories...

5,938 Views
talhamir49
Contributor III

hi @converse  Thanks for your reply.

But I don't think that problem lies in the length of 8k characters as I followed the the provided Document JN-AN1260 to use JN-AN-1246. All the directories names are already set in SDK and example code and locations of IDE SDK and Workspace are set according to the document.

0 Kudos
Reply