The multi-colored LEDs(RGM) of FRDM-KW41Z is not flashing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The multi-colored LEDs(RGM) of FRDM-KW41Z is not flashing

576 Views
xiaoxuan_cai
Contributor I

I have brought a FRDM-KW41Z, but now the multi-colored LEDs(RGB)  is not flashing, that is to say , the board I can only see the two green LEDs are bright.  I unplug and replug in the board, but the multi-colored LEDs(RGB) is still not flashing. How can I do, so that the multi-colored LEDs(RGB)  can flash?

Tags (1)
0 Kudos
Reply
1 Reply

505 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Xiaoxuan Cai,

Seems that you are following the GETTING STARTED of FRDM-KW41Z board.
Not quite sure why the Out-of-Box Demo is not running on your FRDM-KW41Z board.(Maybe some one else has erase the program?)
I think you can go on with Next Step. This step is not much important, and it will not effect next steps.

Out of Box Demo.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply