The SWO Trace function can not be used on the TWR-KE18F board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The SWO Trace function can not be used on the TWR-KE18F board

Jump to solution
631 Views
T2
Contributor III

Hello,

I am using the TWR-KE18F board, but I can not use the SWO Trace function.

The following error message is displayed when using it.
“Failed to configure the probe for SWO-may not be supported with this firmware.”

Is the SWO Trace function not available on the TWR-KE18F board?
Please tell me what to do.

My environment is as follows.
・ TWR-KE18F board
・ MCUXpresso IDE v11.0.0
・ Windows 7 64bit


Best regards.

Labels (1)
1 Solution
506 Views
BlackNight
NXP Employee
NXP Employee

Both your debug connector needs to have the SWO pin available and your debug probe needs to support it (e.g. the LPC-Link2 does support it). Can you check the schematics of your board if that pin is available on the connector?

I hope this helps,

Erich

PS: Tutorial: Using Single Wire Output SWO with ARM Cortex-M and Eclipse | MCU on Eclipse 

View solution in original post

2 Replies
507 Views
BlackNight
NXP Employee
NXP Employee

Both your debug connector needs to have the SWO pin available and your debug probe needs to support it (e.g. the LPC-Link2 does support it). Can you check the schematics of your board if that pin is available on the connector?

I hope this helps,

Erich

PS: Tutorial: Using Single Wire Output SWO with ARM Cortex-M and Eclipse | MCU on Eclipse 

506 Views
T2
Contributor III

Hi Erich,

Thanks for your quick reply.

I checked the TWE-KE18F board schematic.
There was a pin corresponding to SWO.
The contents of the link are very helpful.
Thank you for the advice.

Best regards.

0 Kudos