Hello,
I am using the TWR-KE18F board, but I can not use the SWO Trace function.
The following error message is displayed when using it.
“Failed to configure the probe for SWO-may not be supported with this firmware.”
Is the SWO Trace function not available on the TWR-KE18F board?
Please tell me what to do.
My environment is as follows.
・ TWR-KE18F board
・ MCUXpresso IDE v11.0.0
・ Windows 7 64bit
Best regards.
Solved! Go to Solution.
Both your debug connector needs to have the SWO pin available and your debug probe needs to support it (e.g. the LPC-Link2 does support it). Can you check the schematics of your board if that pin is available on the connector?
I hope this helps,
Erich
PS: Tutorial: Using Single Wire Output SWO with ARM Cortex-M and Eclipse | MCU on Eclipse
Both your debug connector needs to have the SWO pin available and your debug probe needs to support it (e.g. the LPC-Link2 does support it). Can you check the schematics of your board if that pin is available on the connector?
I hope this helps,
Erich
PS: Tutorial: Using Single Wire Output SWO with ARM Cortex-M and Eclipse | MCU on Eclipse
Hi Erich,
Thanks for your quick reply.
I checked the TWE-KE18F board schematic.
There was a pin corresponding to SWO.
The contents of the link are very helpful.
Thank you for the advice.
Best regards.